What are the general layout suggestions when designing the RF section of a PCB?
Answer
Here are some layout hints that are suggested to follow for any kind of RF board designs.
- Use as large and continuous GND metallization as possible on all layers.
- Use plenty of GND stitching vias on the entire PCB, especially at the board and GND metal pouring edges.
- Do not route traces at or close to the board edges.
- Place the high frequency crystal or TCXO close to the RF chip.
- Connect the crystal case to GND.
- Use short VDD traces.
- If possible, shield the VDD traces by ground metallization (with vias) from both sides.
- Put the matching network as close to the RF chip as possible to minimize the parasitics in the RF-FE match and avoid de-tuning.
- Make sure that there are many GND vias on the RF chip's exposed pad.
- If the design uses more than 2 layers it is always recommended to put the VDD line and as many digital traces as possible in an inner layer and use as large and continuous solid ground planes for the top and bottom layers as possible. In this way the top and bottom layers can act like natural shields and the risk of the unwanted harmonic and spur radiation issues can be minimized.
- It is also important to keep the ground plane area under the RF chip and matching network unbroken on the first inner layer.
- Minimize the distance between the neighboring matching components. Move the matching network as close to the RFIC as possible.
- Nearby inductors should be perpendicular to each other in order to avoid the couplings between them.
- Have at least 0.5mm separation between the traces/pads and GND top metal in the RF matching network.
- Place the RF output, antenna far away from any digital lines connected to the RFIC in order to avoid the possibility of latch-up issues (especially in high output power cases). Also, place the antenna far away from any switching, e.g. DCDC, circuitry.
- Have an option for shielding can above the matching/RFIC/XTAL area.
- Always try to follow as much as possible our reference designs' RF layout routing.
- More info can be found in the RF layout guides: AN629/685/791/928.
General RF Layout Routing Suggestions
Question
What are the general layout suggestions when designing the RF section of a PCB?
Answer
Here are some layout hints that are suggested to follow for any kind of RF board designs.
- Use as large and continuous GND metallization as possible on all layers.
- Use plenty of GND stitching vias on the entire PCB, especially at the board and GND metal pouring edges.
- Do not route traces at or close to the board edges.
- Place the high frequency crystal or TCXO close to the RF chip.
- Connect the crystal case to GND.
- Use short VDD traces.
- If possible, shield the VDD traces by ground metallization (with vias) from both sides.
- Put the matching network as close to the RF chip as possible to minimize the parasitics in the RF-FE match and avoid de-tuning.
- Make sure that there are many GND vias on the RF chip's exposed pad.
- If the design uses more than 2 layers it is always recommended to put the VDD line and as many digital traces as possible in an inner layer and use as large and continuous solid ground planes for the top and bottom layers as possible. In this way the top and bottom layers can act like natural shields and the risk of the unwanted harmonic and spur radiation issues can be minimized.
- It is also important to keep the ground plane area under the RF chip and matching network unbroken on the first inner layer.
- Minimize the distance between the neighboring matching components. Move the matching network as close to the RFIC as possible.
- Nearby inductors should be perpendicular to each other in order to avoid the couplings between them.
- Have at least 0.5mm separation between the traces/pads and GND top metal in the RF matching network.
- Place the RF output, antenna far away from any digital lines connected to the RFIC in order to avoid the possibility of latch-up issues (especially in high output power cases). Also, place the antenna far away from any switching, e.g. DCDC, circuitry.
- Have an option for shielding can above the matching/RFIC/XTAL area.
- Always try to follow as much as possible our reference designs' RF layout routing.
- More info can be found in the RF layout guides: AN629/685/791/928.