Si4x6x radios can operate in High-performance or Low-power modes, which can be set in GLOBAL_CONFIG property. In order to save some current consumption (typically 2-3mA), low-power mode can be enabled, however it has some tradeoff in RX performance (sensitivity, linearity).
If the crystal parameters meet the requirements listed in AN785 section 1, both high-performance mode and low-power mode should result robust crystal operation on a properly designed PCB layout (crystal placed as close to the XTAL pins as possible).
In high-performance mode there is some margin on the required crystal parameters, but still it is recommended to stay within the ranges listed in AN785 section 1 for safe operation. Crystal start-up issues might occur if the parameters are not met.
In low-power mode meeting the required crystal parameters is more critical, i.e crystal start-up issues might happen even if the RF crystal parameters are near the edge. Low-power mode can be used robustly with a crystal that easily meets the recommended parameters. AN785 Table 1 provides a list of recommended crystals that will ensure safe operation both in high-performance and low-power mode.
If crystal start-up problem occurs in low-power mode, there are 2 possible options to avoid the issue:
Use the radio in High-performance mode. This will increase RX current by 2-3mA, but sensitivity and range will improve.
Run only the crystal oscillator block in High-performance mode, all other blocks can remain in Low-power mode. This will increase RX current only by 100-200uA, sensitivity will be the same as in Low-power mode, but crystal start-up issues will disappear. In order to do this, after enabling low-performance mode in GLOBAL_CONFIG property, the following bytes should be sent to the radio via SPI interface: "F1 F0 01 5A".
Crystal start-up issue on Si4x6x low-power mode
Si4x6x radios can operate in High-performance or Low-power modes, which can be set in GLOBAL_CONFIG property. In order to save some current consumption (typically 2-3mA), low-power mode can be enabled, however it has some tradeoff in RX performance (sensitivity, linearity).
If the crystal parameters meet the requirements listed in AN785 section 1, both high-performance mode and low-power mode should result robust crystal operation on a properly designed PCB layout (crystal placed as close to the XTAL pins as possible).
In high-performance mode there is some margin on the required crystal parameters, but still it is recommended to stay within the ranges listed in AN785 section 1 for safe operation. Crystal start-up issues might occur if the parameters are not met.
In low-power mode meeting the required crystal parameters is more critical, i.e crystal start-up issues might happen even if the RF crystal parameters are near the edge. Low-power mode can be used robustly with a crystal that easily meets the recommended parameters. AN785 Table 1 provides a list of recommended crystals that will ensure safe operation both in high-performance and low-power mode.
If crystal start-up problem occurs in low-power mode, there are 2 possible options to avoid the issue: