What is the recommended distance between antennas in an antenna diversity application?
Answer
Antennas in a product that implements antenna diversity have their antennas mounted at a distance of at least ¼ wavelength apart. This amount of spatial separation improves the probability that at least one antenna is NOT in a deeply faded signal condition. Another typical recommendation is ½ wavelength antenna distance, however, it can result quite large board sizes at low frequencies (e.g. for 434 MHz frequency ½ wavelength is 34,5 cm).
Can I use the same matching network for EZRadioPRO and an EZR32 wireless MCU that is based on the same radio?
Answer
The answer depends on the actual PCB layer stack-up as the distance between the top and the first inner (ground) layer determines the PCB parasitic capacitances, which plays part in the matching network.
If the same PCB layer stack-up is used (or at least the distance between the top and the first inner layer is similar), in that case the same matching network component values should result very similar TX and RX performance for an EZRadioPRO radio and an EZR32 wireless MCU. If the PCB layer stack-up deviates significantly, it is not recommended to use the same matching network as the detuning can cause lower output power, higher harmonics, higher current consumption and sensitivity loss.
How can I use the EFR32 Series 1 (EFR32xG1x) sub-GHz RF ports in single-ended way?
Answer
Both TX and RX sub-GHz RF ports of EFR32 Series 1 wireless geckos (EFR32xG1x) are truly differential ones. However, they can be used in more simple single-ended way as well, which will enable to use more simple matching networks, but, on the other hand, it will sacrifice some RF performance.
RX:
For single-ended RX operation, sensitivity degradation of 6 dB is expected. The unused input pin can be connected to GND. Note, that it also affects the performance of RFSENSE.
TX:
Regarding the TX, 3 dB lower output power is expected. Also, the harmonic performance will be degraded. The unused TX pin can be connected to GND (to save current).
The single-ended matching network should use halved impedance compared to the differential one, with removed ceramic balun.
The single-ended RX and TX matches use the series elements of the original differential match without any change: i.e. the series capacitor in the RX match and the series inductor in the TX match will remain the same.
The shunt element impedances are halved in the single-ended match and connected to GND: i.e. half shunt inductor value in the RX match and double shunt capacitor values in the TX match are used. As the TX internal capacitor will be small as well an additional external shunt capacitor will be used right at the TX pin as well.
Remove the balun and connect the single ended match output directly to the single ended LPF.
At which pins should I apply DC feed for the sub-GHz and 2.4GHz PA of EFR32 Series 1 devices?
Answer
1. 2.4GHz PA DC feed
The EFR32 Series 1 2.4GHz PA has a dedicated power supply input pin (PAVDD), the 2.4GHz PA should be powered through this pin:
On the sub-GHz side, the PA does not have a dedicated power supply input pin, therefore the sub-GHz PA needs to be powered through the TX output pins: SUBGRF_OP and SUBGRF_ON. Depending on the matching network type and the sub-GHz frequency band, different power supply schemes are needed for the sub-GHz PA:
2. Discrete matching network + ceramic balun for high sub-GHz frequency bands (>500MHz)
For high frequency bands (>500MHz) the recommended ceramic balun type is 0900BL15C050 from Johanson Technology. This balun has a dedicated BIAS input pin, which is in connection with BAL1 and BAL2 pins of the balun, therefore the DC bias will be present on the TX output pins supplying the sub-GHz PA.
An additional VDD filtering capacitor (C10) is required at the BIAS pin of the balun with appropriate value (see the EFR32 Series 1 Reference designs for the proper component values).
3. Discrete matching network + ceramic balun for low sub-GHz frequency bands (<500MHz)
For low frequency bands (<500MHz) the recommended ceramic balun type is ATB2012-50011 from TDK Corporation. This balun has no dedicated BIAS input pin, which means that the PA power supply should be connected to the TX output pins on the other side of the ceramic balun. In order to avoid the PA supply circuit loading the PA matching network, the PA DC feed should be connected to the TX pins through choke inductors (L4 and L5) with appropriate values so that the inductors show high impedance at the frequency of operation.
An additional VDD filtering capacitor (C14) is required at the biasing point prior to the choke inductors (L4 and L5) with appropriate value (see the EFR32 Series 1 Reference designs for the proper component values).
4. Full discrete matching network for any sub-GHz frequency bands
In the full discrete match, the ceramic balun and the TX matching network is replaced by a 4-element discrete balun. The discrete balun contains a shunt inductor (L1), which can be separated into 2 halves, and the PA DC feed can be connected to the common point of these inductors (L1-1 and L1-2). Also, a capacitor for improved 2nd harmonic suppression (CH) is connected at this point.
In order to avoid the PA supply circuit loading the PA matching network, a choke inductor is necessary (LDC).
All 4 IPD types listed in AN1081 have dedicated VDD pins, which are in connection with the TXP and TXN pins of these IPDs, therefore the DC bias will be present on the TX output pins supplying the sub-GHz PA.
Note: When PAVDD (2.4GHz PA) = VBIAS (sub-GHz PA), limiting supply voltage of 2.4GHz PA to transmit at lower power will also limit the supply voltage at sub-GHz. Hence if different max TX power levels are expected from 2.4GHz and sub-GHz PA, then PAVDD and VBIAS net should be supplied separately with appropriate power supply voltages.
In which cases should I apply DC-DC to PAVDD when creating an EFR32 Series 1 design?
Answer
Using the 1.8V output of the internal DC-DC converter of EFR32 Series 1 devices for DC supply of the PA provides better efficiency (i.e. lower PA current for the same output power) compared to the case when the PA is running from the main 3.3V. The recommendation for applying the DC-DC output to PAVDD:
<= 13dBm for 2.4GHz
<= 14dBm for sub-GHz
Above these power levels, using the main 3.3V supply for DC supply of the PA results better efficiency.
Proprietary Knowledge Base
Recommended distance between antennas in an antenna diversity application
Question
What is the recommended distance between antennas in an antenna diversity application?
Answer
Antennas in a product that implements antenna diversity have their antennas mounted at a distance of at least ¼ wavelength apart. This amount of spatial separation improves the probability that at least one antenna is NOT in a deeply faded signal condition. Another typical recommendation is ½ wavelength antenna distance, however, it can result quite large board sizes at low frequencies (e.g. for 434 MHz frequency ½ wavelength is 34,5 cm).
EZRadioPRO vs EZR32 PA matching network
Question
Can I use the same matching network for EZRadioPRO and an EZR32 wireless MCU that is based on the same radio?
Answer
The answer depends on the actual PCB layer stack-up as the distance between the top and the first inner (ground) layer determines the PCB parasitic capacitances, which plays part in the matching network.
If the same PCB layer stack-up is used (or at least the distance between the top and the first inner layer is similar), in that case the same matching network component values should result very similar TX and RX performance for an EZRadioPRO radio and an EZR32 wireless MCU. If the PCB layer stack-up deviates significantly, it is not recommended to use the same matching network as the detuning can cause lower output power, higher harmonics, higher current consumption and sensitivity loss.
EFR32 Series 1 sub-GHz single-ended operation
Question
How can I use the EFR32 Series 1 (EFR32xG1x) sub-GHz RF ports in single-ended way?
Answer
Both TX and RX sub-GHz RF ports of EFR32 Series 1 wireless geckos (EFR32xG1x) are truly differential ones. However, they can be used in more simple single-ended way as well, which will enable to use more simple matching networks, but, on the other hand, it will sacrifice some RF performance.
RX:
For single-ended RX operation, sensitivity degradation of 6 dB is expected. The unused input pin can be connected to GND. Note, that it also affects the performance of RFSENSE.
TX:
Regarding the TX, 3 dB lower output power is expected. Also, the harmonic performance will be degraded. The unused TX pin can be connected to GND (to save current).
The single-ended matching network should use halved impedance compared to the differential one, with removed ceramic balun.
EFR32 Series 1 PA DC feed
Question
At which pins should I apply DC feed for the sub-GHz and 2.4GHz PA of EFR32 Series 1 devices?
Answer
1. 2.4GHz PA DC feed
The EFR32 Series 1 2.4GHz PA has a dedicated power supply input pin (PAVDD), the 2.4GHz PA should be powered through this pin:
On the sub-GHz side, the PA does not have a dedicated power supply input pin, therefore the sub-GHz PA needs to be powered through the TX output pins: SUBGRF_OP and SUBGRF_ON. Depending on the matching network type and the sub-GHz frequency band, different power supply schemes are needed for the sub-GHz PA:
2. Discrete matching network + ceramic balun for high sub-GHz frequency bands (>500MHz)
For high frequency bands (>500MHz) the recommended ceramic balun type is 0900BL15C050 from Johanson Technology. This balun has a dedicated BIAS input pin, which is in connection with BAL1 and BAL2 pins of the balun, therefore the DC bias will be present on the TX output pins supplying the sub-GHz PA.
An additional VDD filtering capacitor (C10) is required at the BIAS pin of the balun with appropriate value (see the EFR32 Series 1 Reference designs for the proper component values).
3. Discrete matching network + ceramic balun for low sub-GHz frequency bands (<500MHz)
For low frequency bands (<500MHz) the recommended ceramic balun type is ATB2012-50011 from TDK Corporation. This balun has no dedicated BIAS input pin, which means that the PA power supply should be connected to the TX output pins on the other side of the ceramic balun. In order to avoid the PA supply circuit loading the PA matching network, the PA DC feed should be connected to the TX pins through choke inductors (L4 and L5) with appropriate values so that the inductors show high impedance at the frequency of operation.
An additional VDD filtering capacitor (C14) is required at the biasing point prior to the choke inductors (L4 and L5) with appropriate value (see the EFR32 Series 1 Reference designs for the proper component values).
4. Full discrete matching network for any sub-GHz frequency bands
In the full discrete match, the ceramic balun and the TX matching network is replaced by a 4-element discrete balun. The discrete balun contains a shunt inductor (L1), which can be separated into 2 halves, and the PA DC feed can be connected to the common point of these inductors (L1-1 and L1-2). Also, a capacitor for improved 2nd harmonic suppression (CH) is connected at this point.
In order to avoid the PA supply circuit loading the PA matching network, a choke inductor is necessary (LDC).
For further details on the full discrete matching solution, see AN1180: EFR32 Series 1 sub-GHz Discrete Matching Solutions.
5. IPD matching network for any sub-GHz frequency bands
EFR32 Series 1 IPDs are available for 434MHz and 868MHz frequency bands, see additional details in AN1081: Integrated Passive Devices for EFR32 Series 1 Sub-GHz RF Matching.
All 4 IPD types listed in AN1081 have dedicated VDD pins, which are in connection with the TXP and TXN pins of these IPDs, therefore the DC bias will be present on the TX output pins supplying the sub-GHz PA.
Note: When PAVDD (2.4GHz PA) = VBIAS (sub-GHz PA), limiting supply voltage of 2.4GHz PA to transmit at lower power will also limit the supply voltage at sub-GHz. Hence if different max TX power levels are expected from 2.4GHz and sub-GHz PA, then PAVDD and VBIAS net should be supplied separately with appropriate power supply voltages.
EFR32 Series 1 DC-DC to PAVDD
Question
In which cases should I apply DC-DC to PAVDD when creating an EFR32 Series 1 design?
Answer
Using the 1.8V output of the internal DC-DC converter of EFR32 Series 1 devices for DC supply of the PA provides better efficiency (i.e. lower PA current for the same output power) compared to the case when the PA is running from the main 3.3V. The recommendation for applying the DC-DC output to PAVDD:
Above these power levels, using the main 3.3V supply for DC supply of the PA results better efficiency.