Si4362 revB1B Command/Property API Documentation
Interface Version: 1.0
Document Version: 2.0.5
Generated: 2015-03-18T10:15:42-05:00
Introduction
This document provides API descriptions for the commands and properties used
to control and configure the part. The interface version tracks any functional
changes to the API (command, property, field, enumeration, etc.). The documentation
version tracks any text changes to the summary or description text of the API
components.
The commands are listed in a summary table with links to command details.
The properties are listed in a summary
table with links to property details. The feature available column in the
summary tables lists the firmware revision which first implemented the command
or property.
An entry in the summary table will link
to a details section, which contains a register view with fields. Clicking a
field in the register view will auto-expand the corresponding field details.
An up button in the field detail links back to the register view. Each
register view title links back to the summary table entry. These hyper-links
provide two-click access from top to bottom.
Command Summary
  |
|
0x02 |
POWER_UP
|
Command to power-up the device and select the operational mode and functionality. |
|
  |
|
0x00 |
NOP
|
No Operation command. |
|
|
0x01 |
PART_INFO
|
Reports basic information about the device. |
|
|
0x10 |
FUNC_INFO
|
Returns the Function revision information of the device. |
|
|
0x44 |
READ_CMD_BUFF
|
Used to read CTS and the command response. |
|
  |
|
0x23 |
GET_CHIP_STATUS
|
Returns the interrupt status of the Chip Interrupt Group (both STATUS and PENDING). Optionally, it may be used to clear latched (PENDING) interrupt events. |
|
Property Summary
Command Details
- Number: 0x02
- Summary: Command to power-up the device and select the operational mode and functionality.
- Purpose:
- Argument Stream:
- Reply Stream:
- Argument Fields:
- Description:
- Select patch mode or normal boot mode.
- Format:
- Enumeration
| Name |
Value |
Description |
Feature Available |
| NO_PATCH |
0 |
Power up into functional mode specified by FUNC parameter. |
|
| PATCH |
1 |
Indicates a patch has been applied. Validate patch matches the function selected (indicated by the FUNC parameter) and boot the device. |
|
- Description:
- Selects the functionality of the device by specifying the firmware image to be loaded upon boot-up.
- Format:
- Enumeration
| Name |
Value |
Description |
Feature Available |
- Description:
- Specifies the frequency of the internal crystal oscillator or external TCXO in Hz. The nominal value is 30000000 (30 MHz) = 0x01C9C380.
- This parameter is used during calibration of the Boot Clock Oscillator and 32kHz R-C Oscillator, but is NOT used for calibration or tuning of the PLL Synthesizer.
- Type:
- U32
- Min:
- 0x17d7840
- Max:
- 0x1e84800
- Reply Fields:
- Description:
- Clear to Send. Indicates that the previous command has completed execution and the response byte stream (if any) is valid. The next command may be sent.
- Type:
- U8
- Number: 0x00
- Summary: No Operation command.
- Purpose:
- This command may be used to ensure that communication with the device has been established. Upon receipt of this command, the chip performs no action except to return CTS.
- Argument Stream:
- Reply Stream:
- Argument Fields:
- Reply Fields:
- Description:
- Clear to Send. Indicates that the previous command has completed execution and the response byte stream (if any) is valid. The next command may be sent.
- Type:
- U8
- Number: 0x01
- Summary: Reports basic information about the device.
- Purpose:
- Returns Part Number, Part Version, ROM ID, etc.
- Argument Stream:
- Reply Stream:
- Argument Fields:
- Reply Fields:
- Description:
- Clear to Send. Indicates that the previous command has completed execution and the response byte stream (if any) is valid. The next command may be sent.
- Type:
- U8
- Description:
- Chip Mask Revision.
- Type:
- U8
- Description:
- Part Number (e.g., si4461 will return - 0x4461).
- Type:
- U16
- Description:
- Part Build.
- Type:
- U8
- Description:
- Id.
- Type:
- U16
- Description:
- Customer ID.
- Type:
- U8
- Description:
- ROM Id.
- Type:
- U8
- Number: 0x10
- Summary: Returns the Function revision information of the device.
- Purpose:
- Return Function revision numbers for currently loaded functional mode. Contrast with PART_INFO.
- Argument Stream:
- Reply Stream:
- Argument Fields:
- Reply Fields:
- Description:
- Clear to Send. Indicates that the previous command has completed execution and the response byte stream (if any) is valid. The next command may be sent.
- Type:
- U8
- Description:
- External revision number.
- Type:
- U8
- Min:
- 0x0
- Max:
- 0xff
- Description:
- Branch revision number.
- Type:
- U8
- Min:
- 0x0
- Max:
- 0xff
- Description:
- Internal revision number.
- Type:
- U8
- Min:
- 0x0
- Max:
- 0xff
- Description:
- ID of applied patch. This is also the last 2 bytes in the associated patch file (*.csg).
- 0x0000 = No patch applied.
- Type:
- U16
- Description:
- Current functional mode.
- Type:
- U8
- Number: 0x44
- Summary: Used to read CTS and the command response.
- Purpose:
- Processing of API commands is handled by the command handler in the chip. A subsequent command may not be sent until the chip has completed processing of the first command. The chip indicates the ability to receive another command and the availability of response data by issuing a Clear To Send (CTS) signal; it is necessary for the host MCU to poll the chip for this CTS signal. The CTS signal may be polled via SPI command, or monitored on a GPIO line or as an interrupt on the nIRQ pin.
- This command is used to poll the CTS signal via the SPI bus. The NSEL line should be pulled low, followed by sending the READ_CMD_BUFF command on SDI. While NSEL remains asserted low, an additional eight clock pulses are sent on SCLK and the CTS response byte is read on SDO. If the CTS response byte is not 0xFF, the host MCU should pull NSEL high and repeat the polling procedure.
- If the CTS response byte is 0xFF, the host MCU should keep NSEL asserted low and provide additional clock cycles on SCLK to read out as many response bytes (on SDO) as necessary. The host MCU should pull NSEL high upon completion of reading the response stream.
- A primary function of this command is to determine when CTS goes high, and thus by definition this command may be sent while CTS is low. This command itself does not cause CTS to go low.
- Attempting to read response bytes from the command buffer while CTS is not 0xFF will return invalid results. The response bytes are valid only if CTS = 0xFF.
- Argument Stream:
- Reply Stream:
- Argument Fields:
- Reply Fields:
- Description:
- Clear to Send. Indicates that the previous command has completed execution and the response byte stream (if any) is valid. The next command may be sent.
- Type:
- U8
- Description:
- Byte 0-15 of the command response buffer.
- Type:
- U8
- Number: 0x23
- Summary: Returns the interrupt status of the Chip Interrupt Group (both STATUS and PENDING). Optionally, it may be used to clear latched (PENDING) interrupt events.
- Purpose:
- Returns the current interrupt status of Chip interrupt events (both STATUS and PENDING) and optionally clears PENDING interrupts.
- Please refer to the GET_INT_STATUS command for more details regarding the difference between STATUS and PENDING interrupts.
- Sending the GET_CHIP_STATUS command with NO input parameter results in clearing all of the PENDING interrupts.
- When PENDING interrupts are being cleared, the reply stream reflects their status prior to clearing.
- Argument Stream:
- Reply Stream:
- Argument Fields:
- Description:
- If clear, clear any pending CAL interrupt. If set, leave interrupt pending.
- Type:
- BOOL
- Description:
- If clear, clear any pending FIFO_UNDERFLOW_OVERFLOW_ERROR interrupt. If set, leave interrupt pending.
- Type:
- BOOL
- Description:
- If clear, clear any pending STATE_CHANGE interrupt. If set, leave interrupt pending.
- Type:
- BOOL
- Description:
- If clear, clear any pending CMD_ERROR interrupt. If set, leave interrupt pending.
- Type:
- BOOL
- Description:
- If clear, clear any pending CHIP_READY interrupt. If set, leave interrupt pending.
- Type:
- BOOL
- Description:
- If clear, clear any pending LOW_BATT interrupt. If set, leave interrupt pending.
- Type:
- BOOL
- Description:
- If clear, clear any pending WUT interrupt. If set, leave interrupt pending.
- Type:
- BOOL
- Reply Fields:
- Description:
- Clear to Send. Indicates that the previous command has completed execution and the response byte stream (if any) is valid. The next command may be sent.
- Type:
- U8
- Description:
- If set, a rising edge of the CAL status bit has been detected and therefore a CAL interrupt is pending. See associated CAL status bit for more details.
- Type:
- BOOL
- Description:
- If set, a rising edge of the FIFO_UNDERFLOW_OVERFLOW_ERROR status bit has been detected and therefore a FIFO_UNDERFLOW_OVERFLOW_ERROR interrupt is pending. See associated FIFO_UNDERFLOW_OVERFLOW_ERROR status bit for more details.
- Type:
- BOOL
- Description:
- If set, a rising edge of the STATE_CHANGE status bit has been detected and therefore a STATE_CHANGE interrupt is pending. See associated STATE_CHANGE status bit for more details.
- Type:
- BOOL
- Description:
- If set, a rising edge of the CMD_ERROR status bit has been detected and therefore a CMD_ERROR interrupt is pending. See associated CMD_ERROR status bit for more details.
- Type:
- BOOL
- Description:
- If set, a rising edge of the CHIP_READY status bit has been detected and therefore a CHIP_READY interrupt is pending. See associated CHIP_READY status bit for more details.
- Type:
- BOOL
- Description:
- If set, a rising edge of the LOW_BATT status bit has been detected and therefore a LOW_BATT interrupt is pending. See associated LOW_BATT status bit for more details.
- Type:
- BOOL
- Description:
- If set, a rising edge of the WUT status bit has been detected and therefore a WUT interrupt is pending. See associated WUT status bit for more details.
- Type:
- BOOL
- Description:
- Self clearing signal that pulses high to indicate a RC32K calibration event is pending. If this occurs, the RC32K oscillator will be calibrated on the next transition to Sleep/Standby state.
- Type:
- BOOL
- Description:
- Set to indicate that the number of received or transmitted bytes exceeds the size of the RX or TX FIFO, respectively (i.e., 64 bytes for each FIFO, or 129 bytes when sharing the FIFO). Upon such an underflow/overflow event, the FIFO(s) will need to be reset. Cleared by issuing a FIFO_INFO command to reset the FIFOs.
- Type:
- BOOL
- Description:
- Set to indicate a successful transition from one state to another operating state. Cleared when a state transition is in progress.
- Type:
- BOOL
- Description:
- Self clearing signal that pulses high to indicate an error has occurred in the processing of a command. For example, an incorrect command/property ID is sent, or an attempt was made to write a property that is outside of the given property group.
- Type:
- BOOL
- Description:
- Set to indicate the chip (upon completion of the POWER_UP sequence) has reached the state where it is ready to accept commands, or when the IR calibration process is completed. Cleared when the chip is shutdown or when IR calibration has begun.
- Type:
- BOOL
- Description:
- Self clearing signal that pulses high to indicate the WUT (Wake-up timer) has expired.
- Type:
- BOOL
- Description:
- Last command error cause. Only valid if CMD_ERROR status bit is set.
- Format:
- Enumeration
| Name |
Value |
Description |
Feature Available |
| CMD_ERROR_NONE |
0 |
No error. |
|
| CMD_ERROR_BAD_COMMAND |
16 |
Bad command issued. |
|
| CMD_ERROR_BAD_ARG |
17 |
Argment(s) in issued command were invalid. |
|
| CMD_ERROR_COMMAND_BUSY |
18 |
Command was issued before previous command was completed. |
|
| CMD_ERROR_BAD_BOOTMODE |
49 |
Invalid bootmode supplied. |
|
| CMD_ERROR_BAD_PROPERTY |
64 |
Bad Property ID was provided. |
|
- Description:
- Command ID that was being proccessed at the time of the last command error.
- Type:
- ENUM
Property Details