See more details at http://www.yolinux.com/TUTORIALS/LibraryArchives-StaticAndDynamic.html

To link against a shared object library (.so) using -l<libraryname>:
1. Copy the library built from the project to /opt/lib:

  $ mkdir -p /opt/lib
  $ cp libslabhidtouart.so.1.0 /opt/lib/

2. Create a .so link:

  $ ln -sf /opt/lib/libslabhidtouart.so.1.0 /opt/lib/libslabhidtouart.so

3. Create a .so.1 link:

  $ ln -sf /opt/lib/libslabhidtouart.so.1.0 /opt/lib/libslabhidtouart.so.1

To run an executable that was built against the shared object library (.so):
1. Set the library path to /obt/lib before running the executable
   example: export LD_LIBRARY_PATH=/opt/lib:$LD_LIBRARY_PATH

To list the dependencies of an object file or binary:
example: ldd main

To view a list of exported symbols from an object file or library:
example: nm -D libslabhidtouart.so.1.0
example (paginate displayed results): nm -D libslabadi.so.1.0 | less