/** \file
 *
 *  This file contains special DoxyGen information for the generation of the main page and other special
 *  documentation pages. It is not a project source file.
 */

/** \mainpage Communications Device Class (Virtual Serial Port) Demo
 *
 *  \section Sec_Compat Demo Compatibility:
 *
 *  The following list indicates what microcontrollers are compatible with this demo.
 *
 *  \li EFM32 GiantGecko (EFM32F990GG)
 *
 *  \section Sec_Info USB Information:
 *
 *  The following table gives a rundown of the USB utilization of this demo.
 *
 *  <table>
 *   <tr>
 *    <td><b>USB Mode:</b></td>
 *    <td>Device</td>
 *   </tr>
 *   <tr>
 *    <td><b>USB Class:</b></td>
 *    <td>Communications Device Class (CDC)</td>
 *   </tr>
 *   <tr>
 *    <td><b>USB Subclass:</b></td>
 *    <td>Abstract Control Model (ACM)</td>
 *   </tr>
 *   <tr>
 *    <td><b>Relevant Standards:</b></td>
 *    <td>USBIF CDC Class Standard</td>
 *   </tr>
 *   <tr>
 *    <td><b>Supported USB Speeds:</b></td>
 *    <td>Full Speed Mode</td>
 *   </tr>
 *  </table>
 *
 *  \section Sec_Description Project Description:
 *
 *  Communications Device Class demonstration application.
 *  This gives a simple reference application for implementing
 *  a CDC device acting as a virtual serial port. Joystick
 *  actions are transmitted to the host as strings. The device
 *  does not respond to serial data sent from the host.
 *
 *  After running this demo for the first time on a new computer,
 *  you will need to supply the .INF file located in this demo
 *  project's directory as the device's driver when running under
 *  Windows. This will enable Windows to use its inbuilt CDC drivers,
 *  negating the need for custom drivers for the device. Other
 *  Operating Systems should automatically use their own inbuilt
 *  CDC-ACM drivers.
 *
 *  \section Sec_Options Project Options
 *
 *  The following defines can be found in this demo, which can control the demo behaviour when defined, or changed in value.
 *
 *  <table>
 *   <tr>
 *    <td>
 *     None
 *    </td>
 *   </tr>
 *  </table>
 */