The ATPROGRAM programming utility LUFA build system module, providing targets to reprogram an Atmel processor FLASH and EEPROM memories with a project's compiled binary output files.
To use this module in your application makefile, add the following code:
include $(LUFA_PATH)/Build/lufa_atprogram.mk
Requirements
This module requires the atprogram.exe utility to be available in your system's PATH variable. The atprogram.exe utility is distributed in Atmel AVR Studio 5.x and Atmel Studio 6.x inside the application install folder's "\atbackend" subdirectory.
Targets
atprogram | Program the device FLASH memory with the application's executable data. |
atprogram-ee | Program the device EEPROM memory with the application's EEPROM data. |
Mandatory Parameters
MCU | Name of the Atmel processor model (e.g. at90usb1287). |
TARGET | Name of the application output file prefix (e.g. TestApplication). |
Optional Parameters
ATPROGRAM_PROGRAMMER | Name of the Atmel programmer or debugger tool to communicate with (e.g. jtagice3). |
ATPROGRAM_INTERFACE | Name of the programming interface to use when programming the target (e.g. spi). |
ATPROGRAM_PORT | Name of the communication port to use when when programming with a serially connected tool (e.g. COM2). |
Module Provided Variables
Module Provided Macros