The DOXYGEN code documentation utility LUFA build system module, providing targets to generate project HTML and other format documentation from a set of source files that include special Doxygen comments.
To use this module in your application makefile, add the following code:
include $(LUFA_PATH)/Build/lufa_doxygen.mk
Requirements
This module requires the doxygen utility from the Doxygen website (http://www.doxygen.org/) to be available in your system's PATH variable. On *nix systems the doxygen utility can be installed via the project's source code or through the package manager.
Targets
doxygen | Generate project documentation. |
doxygen_create | Create a new Doxygen configuration file using the latest template. |
doxygen_upgrade | Upgrade an existing Doxygen configuration file to the latest template |
Mandatory Parameters
LUFA_PATH | Path to the LUFA library core, either relative or absolute (e.g. ../LUFA-000000/LUFA/). |
Optional Parameters
DOXYGEN_CONF | Name and path of the base Doxygen configuration file for the project. |
DOXYGEN_FAIL_ON_WARNING | Set to Y to fail the generation with an error exit code if warnings are found other than unsupported configuration parameters, N to continue without failing. |
DOXYGEN_OVERRIDE_PARAMS | Extra Doxygen configuration parameters to apply, overriding the corresponding config entry in the project's configuration file (e.g. QUIET=YES). |
Module Provided Variables
Module Provided Macros