The HID programming utility LUFA build system module, providing targets to reprogram an Atmel processor's FLASH memory with a project's compiled binary output file. This module requires a HID class bootloader to be running in the target, using a protocol compatible with the PJRC "HalfKay" protocol (http://www.pjrc.com/teensy/halfkay_protocol.html).
To use this module in your application makefile, add the following code:
include $(LUFA_PATH)/Build/lufa_hid.mk
Requirements
This module requires either the hid_bootloader_cli utility from the included LUFA HID class bootloader API subdirectory, or the teensy_loader_cli utility from PJRC (http://www.pjrc.com/teensy/loader_cli.html) to be available in your system's PATH variable.
Targets
hid | Program the device FLASH memory with the application's executable data using hid_bootloader_cli. |
hid-ee | Program the device EEPROM memory with the application's EEPROM data using hid_bootloader_cli and a temporary AVR application programmed into the target's FLASH. - Note
- This will erase the currently loaded application in the target.
|
teensy | Program the device FLASH memory with the application's executable data using teensy_loader_cli. |
teensy-ee | Program the device EEPROM memory with the application's EEPROM data using teensy_loader_cli and a temporary AVR application programmed into the target's FLASH. - Note
- This will erase the currently loaded application in the target.
|
Mandatory Parameters
MCU | Name of the Atmel processor model (e.g. at90usb1287). |
TARGET | Name of the application output file prefix (e.g. TestApplication). |
Optional Parameters
Module Provided Variables
Module Provided Macros