The SOURCES LUFA build system module, providing variables listing the various LUFA source files required to be build by a project for a given LUFA module. This module gives a way to reference LUFA source files symbolically, so that changes to the library structure do not break the library makefile.
To use this module in your application makefile, add the following code:
include $(LUFA_PATH)/Build/lufa_sources.mk
Requirements
None.
Targets
Mandatory Parameters
LUFA_PATH | Path to the LUFA library core, either relative or absolute (e.g. ../LUFA-000000/LUFA/). |
ARCH | Architecture of the target processor (see Device and Hardware Support). |
Optional Parameters
Module Provided Variables
LUFA_SRC_USB | List of LUFA USB driver source files. |
LUFA_SRC_USBCLASS | List of LUFA USB Class driver source files. |
LUFA_SRC_TEMPERATURE | List of LUFA temperature sensor driver source files. |
LUFA_SRC_SERIAL | List of LUFA Serial U(S)ART driver source files. |
LUFA_SRC_TWI | List of LUFA TWI driver source files. |
LUFA_SRC_PLATFORM | List of LUFA architecture specific platform management source files. |
Module Provided Macros