If the target microcontroller model, architecture, clock speed, board or other settings are different from the current settings, they must be changed and the project recompiled from the source code before being programmed into the microcontroller. Most project configuration options are located in the makefile build script inside each LUFA application's folder, however some demo or application-specific configuration settings are located in one or more of the source files of the project. See each project's individual documentation for application-specific configuration values.
Each project "makefile" contains all the script and configuration data required to compile each project. When opened with any regular basic text editor such as Notepad or WordPad (ensure that the save format is a pure ASCII text format) the build configuration settings may be altered.
Below is a copy of the default LUFA application makefile, which can be used as a template for each application.
# # LUFA Library # Copyright (C) Dean Camera, 2014. # # dean [at] fourwalledcubicle [dot] com # www.lufa-lib.org # # -------------------------------------- # LUFA Project Makefile. # -------------------------------------- # Run "make help" for target help. MCU = at90usb1287 ARCH = AVR8 BOARD = USBKEY F_CPU = 8000000 F_USB = $(F_CPU) OPTIMIZATION = s TARGET = Target SRC = $(TARGET).c $(LUFA_SRC_USB) $(LUFA_SRC_USBCLASS) $(LUFA_SRC_PLATFORM) LUFA_PATH = ../../LUFA CC_FLAGS = -DUSE_LUFA_CONFIG_HEADER -IConfig LD_FLAGS = # Default target all: # Include LUFA build script makefiles include $(LUFA_PATH)/Build/lufa_core.mk include $(LUFA_PATH)/Build/lufa_sources.mk include $(LUFA_PATH)/Build/lufa_build.mk include $(LUFA_PATH)/Build/lufa_cppcheck.mk include $(LUFA_PATH)/Build/lufa_doxygen.mk include $(LUFA_PATH)/Build/lufa_dfu.mk include $(LUFA_PATH)/Build/lufa_hid.mk include $(LUFA_PATH)/Build/lufa_avrdude.mk include $(LUFA_PATH)/Build/lufa_atprogram.mk
Inside each makefile, a number of configuration variables are listed with the syntax "<VARIABLE NAME> = <VALUE>". For each application, the important standard variables which should be altered are:
These values should be changed to reflect the build hardware.
This parameter indicates the target microcontroller model for the compiled application. This should be set to the model of the target microcontroller (such as the AT90USB1287, or the ATMEGA32U4), in all lower-case (e.g. "at90usb1287"). Note that not all demos support all the microcontroller models and architectures, as they may make use of peripherals or modes only present in some devices.
For supported processor models, see Device and Hardware Support.
This parameter indicates the target microcontroller architecture the library is to be compiled for. Different microcontroller architectures require different source files to be compiled into the final binary, and so this option must be set to the correct architecture for the selected platform.
For supported processor architectures, see Device and Hardware Support.
This parameter indicates the target board hardware for the compiled application. Some LUFA library drivers are board-specific, such as the LED driver, and the library needs to know the layout of the target board. If you are using one of the board models listed on the main library page, change this parameter to the board name in all UPPER-case.
If you are not using any board-specific drivers in the LUFA library, or you are using a custom board layout, change this to read "USER" (no quotes) instead of a standard board name. If the USER board type is selected and the application makes use of one or more board-specific hardware drivers inside the LUFA library, then the appropriate stub drives files should be copied from the /CodeTemplates/DriverStubs/ directory into a /Board/ folder inside the application directory, and the stub driver completed with the appropriate code to drive the custom board's hardware.
For boards with built in hardware driver support within the LUFA library, see Device and Hardware Support.
This parameter indicates the target microcontroller's main CPU clock frequency, in Hz. This is used by many libraries (and applications) for timing related purposes, and should reflect the actual CPU speed after any prescaling or adjustments are performed.
This parameter indicates the raw input clock frequency to the USB module within the microcontroller in Hz. This may be very different on some platforms to the main CPU clock or other peripheral/bus clocks.
This parameter indicates the level of optimization to use when compiling the application. This will allow you to compile with an optimization level supported by GCC, from 0 (no optimization) to 3 (fastest runtime optimization) or s (smallest size).
This parameter indicates the application target name, which is used as the base filename for the build binary and debugging files. This will be the name of the output files once linked together into the final application, ready to load into the target.
This parameter indicates the source files used to compile the application, as a list of C (*.c), C++ (*.cpp) and Assembly (*.S) files. Note that all assembly files must end in a capital .S extension, as lowercase .s files are reserved for GCC intermediate files.
As each LUFA program requires the LUFA library source code to compile correctly, the application must know where the LUFA library is located. This value specifies the path to the LUFA library core. This path may be relative or absolute, however note than even under Windows based systems the forward-slash (/) path separator must be used.
This parameter lists the compiler flags passed to the C/C++ compiler, the assembler and the linker. These are used as-is directly to GCC and thus must match GCC's command line options as given in the GCC manual. This variable may be used to define tokens directly on the command line, enable or disable warnings, adjust the target-specific tuning parameters or other options.
This parameter lists the linker flags passed exclusively to the linker. These are used as-is directly to GCC and thus must match GCC's command line linker options as given in the GCC manual. This variable may be used to create or relocate custom data sections, or enable linker specific behaviors.