The LUFA library uses VID/PID combinations generously donated by Atmel. The following VID/PID combinations are used within the LUFA demos, and thus may be re-used by derivations of each demo. Free PID values may be used by future LUFA demo projects.
These VID/PID values should not be used in commercial designs under any circumstances. Private projects may use the following values freely, but must accept any collisions due to other LUFA derived private projects sharing identical values. It is suggested that private projects using interfaces compatible with existing demos share the same VID/PID value.
| VID | PID | Usage |
|---|---|---|
| 0x03EB | 0x2040 | Test VID/PID (See The Test VID/PID Combination) |
| 0x03EB | 0x2041 | Mouse Demo Application |
| 0x03EB | 0x2042 | Keyboard Demo Application |
| 0x03EB | 0x2043 | Joystick Demo Application |
| 0x03EB | 0x2044 | CDC Demo Application |
| 0x03EB | 0x2045 | Mass Storage Demo Application |
| 0x03EB | 0x2046 | Audio Output Demo Application |
| 0x03EB | 0x2047 | Audio Input Demo Application |
| 0x03EB | 0x2048 | MIDI Demo Application |
| 0x03EB | 0x2049 | MagStripe Project |
| 0x03EB | 0x204A | CDC Class Bootloader |
| 0x03EB | 0x204B | USB to Serial Demo Application |
| 0x03EB | 0x204C | RNDIS Demo Application |
| 0x03EB | 0x204D | Combined Keyboard and Mouse Demo Application |
| 0x03EB | 0x204E | Dual CDC Demo Application |
| 0x03EB | 0x204F | Generic HID Demo Application |
| 0x03EB | 0x2060 | Benito Programmer Project |
| 0x03EB | 0x2061 | Combined Mass Storage and Keyboard Demo |
| 0x03EB | 0x2062 | Combined CDC and Mouse Demo |
| 0x03EB | 0x2063 | Mass Storage/HID Interface Datalogger Project |
| 0x03EB | 0x2064 | Interfaceless Control-Only LUFA Devices |
| 0x03EB | 0x2065 | Test and Measurement Demo |
| 0x03EB | 0x2066 | Multiple Report Keyboard/Mouse HID Demo |
| 0x03EB | 0x2067 | HID Class Bootloader |
| 0x03EB | 0x2068 | Virtual Serial/Mass Storage Demo |
| 0x03EB | 0x2069 | Webserver Project |
| 0x03EB | 0x206A | Media Control Project |
| 0x03EB | 0x206B | Printer Class Bootloader |
| 0x03EB | 0x206C | Bulk Vendor Demo |
| 0x03EB | 0x206D | Currently Unallocated |
| 0x03EB | 0x206E | Currently Unallocated |
| 0x03EB | 0x206F | Currently Unallocated |
For use in testing of LUFA powered devices during development only, by non-commercial entities. All devices must accept collisions on this VID/PID range (from other in-development LUFA devices) to be resolved by using a unique release number in the Device Descriptor. No devices using this VID/PID combination may be released to the general public.