Supported pre-made board hardware defines. More...
Board macros for indicating the chosen physical board hardware to the library. These macros should be used when defining the BOARD token to the chosen hardware via the -D switch in the project makefile. If a custom board is used, the BOARD_NONE or BOARD_USER values should be selected.
| #define BOARD_A3BU_XPLAINED 31 |
Selects the Atmel XMEGA A3BU Xplained specific board drivers, including Dataflash, Button and LED drivers.
| #define BOARD_ADAFRUITU4 23 |
Selects the Adafruit U4 specific board drivers, including the Button driver.
| #define BOARD_ATAVRUSBRF01 6 |
Selects the ATAVRUSBRF01 specific board drivers, including the driver for the board LEDs.
| #define BOARD_B1_XPLAINED 44 |
Selects the XMEGA B1 Xplained specific board drivers, including the Button and LED drivers.
| #define BOARD_BENITO 13 |
Selects the Benito specific board drivers, including the Button and LEDs drivers.
| #define BOARD_BIGMULTIO 46 |
Selects the Bitwizard Big-Multio specific board drivers, including the driver for the board LEDs.
| #define BOARD_BLACKCAT 20 |
Selects the Blackcat USB JTAG specific board drivers, including the driver for the board LEDs.
| #define BOARD_BUI 17 |
Selects the BUI specific board drivers, including the driver for the board LEDs.
| #define BOARD_BUMBLEB 7 |
Selects the BUMBLEB specific board drivers, using the officially recommended peripheral layout.
| #define BOARD_C3_XPLAINED 55 |
Selects the XMEGA C3 XPLAINED specific board drivers, including the Button and LEDs drivers.
| #define BOARD_CULV3 19 |
Selects the Busware CUL V3 specific board drivers, including the Button and LEDs drivers.
| #define BOARD_DK3750 58 |
Selects the STK3750 specific board drivers, including Button, LEDs and UART drivers.
| #define BOARD_DUCE 47 |
Selects the DorkbotPDX Duce specific board drivers, including the driver for the board LEDs.
| #define BOARD_EVK1100 29 |
Selects the Atmel EVK1100 specific board drivers, including the Button, Joystick and LED drivers.
| #define BOARD_EVK1101 27 |
Selects the Atmel EVK1101 specific board drivers, including the Button, Joystick and LED drivers.
| #define BOARD_EVK1104 30 |
Selects the Atmel EVK1104 specific board drivers, including the Button and LED drivers.
| #define BOARD_EVK527 10 |
Selects the EVK527 specific board drivers, including Temperature, Button, Dataflash, Joystick and LED drivers.
| #define BOARD_JMDBU2 14 |
Selects the JM-DB-U2 specific board drivers, including the Button and LEDs drivers.
| #define BOARD_LEONARDO 51 |
Selects the Arduino Leonardo specific board drivers, including the driver for the board LEDs.
| #define BOARD_MAXIMUS 21 |
Selects the Maximus specific board drivers, including the driver for the board LEDs.
| #define BOARD_MICROPENDOUS_1 37 |
Selects the Micropendous 1 specific board drivers, including the driver for the board Button.
| #define BOARD_MICROPENDOUS_2 38 |
Selects the Micropendous 2 specific board drivers, including the driver for the board Button.
| #define BOARD_MICROPENDOUS_3 39 |
Selects the Micropendous 3 specific board drivers, including the driver for the board Button.
| #define BOARD_MICROPENDOUS_32U2 35 |
Selects the Micropendous 32U2 specific board drivers, including the Button and LED drivers.
| #define BOARD_MICROPENDOUS_4 40 |
Selects the Micropendous 4 specific board drivers, including the driver for the board Button.
| #define BOARD_MICROPENDOUS_A 36 |
Selects the Micropendous A specific board drivers, including the driver for the board Button.
| #define BOARD_MICROPENDOUS_DIP 41 |
Selects the Micropendous DIP specific board drivers, including the driver for the board Button.
| #define BOARD_MICROPENDOUS_REV1 42 |
Selects the Micropendous (Arduino-like) revision 1 specific board drivers, including the Button and LED drivers.
| #define BOARD_MICROPENDOUS_REV2 43 |
Selects the Micropendous (Arduino-like) revision 2 specific board drivers, including the Button and LED drivers.
| #define BOARD_MICROSIN162 24 |
Selects the Microsin AVR-USB162 specific board drivers, including the Button and LEDs drivers.
| #define BOARD_MINIMUS 22 |
Selects the Minimus specific board drivers, including the Button and LEDs drivers.
| #define BOARD_MULTIO 45 |
Selects the Bitwizard Multio specific board drivers, including the driver for the board LEDs.
| #define BOARD_NONE 1 |
Disables board drivers when operation will not be adversely affected (e.g. LEDs) - use of board drivers such as the Joystick driver, where the removal would adversely affect the code's operation is still disallowed.
| #define BOARD_OLIMEX162 15 |
Selects the Olimex AVR-USB-162 specific board drivers, including the Button and LEDs drivers.
| #define BOARD_OLIMEX32U4 48 |
Selects the Olimex AVR-USB-32U4 specific board drivers, including the Button and LED drivers.
| #define BOARD_OLIMEXISPMK2 50 |
Selects the Olimex AVR-ISP-MK2 specific board drivers, including the Button and LED drivers.
| #define BOARD_OLIMEXT32U4 49 |
Selects the Olimex AVR-USB-T32U4 specific board drivers, including the Button and LED drivers.
| #define BOARD_RZUSBSTICK 5 |
Selects the RZUSBSTICK specific board drivers, including the driver for the boards LEDs.
| #define BOARD_SPARKFUN8U2 26 |
Selects the Sparkfun ATMEGA8U2 specific board drivers, including the driver for the board LEDs.
| #define BOARD_STANGE_ISP 54 |
Selects the Stange-ISP specific board drivers, including the Button and LEDs drivers.
| #define BOARD_STK3700 57 |
Selects the STK3700 specific board drivers, including Button, LEDs and UART drivers.
| #define BOARD_STK525 3 |
Selects the STK525 specific board drivers, including Temperature, Button, Dataflash, Joystick and LED drivers.
| #define BOARD_STK526 4 |
Selects the STK526 specific board drivers, including Temperature, Button, Dataflash, Joystick and LED drivers.
| #define BOARD_TEENSY 11 |
Selects the Teensy version 1.x specific board drivers, including the driver for the board LEDs.
| #define BOARD_TEENSY2 32 |
Selects the Teensy version 2.x specific board drivers, including the driver for the board LEDs.
| #define BOARD_TUL 28 |
Selects the Busware TUL specific board drivers, including the Button and LED drivers.
| #define BOARD_U2S 56 |
Selects the U2S specific board drivers, including the Button and LEDs drivers.
| #define BOARD_UC3A3_XPLAINED 52 |
Selects the UC3-A3 Xplained specific board drivers, including the Button and LED drivers.
| #define BOARD_UDIP 16 |
Selects the UDIP specific board drivers, including the Button and LEDs drivers.
| #define BOARD_UNO 18 |
Selects the Arduino Uno specific board drivers, including the driver for the board LEDs.
| #define BOARD_USB2AX 33 |
Selects the USB2AX version 1 and 2 specific board drivers, including the Button and LEDs drivers.
| #define BOARD_USB2AX_V3 34 |
Selects the USB2AX version 3 specific board drivers, including the Button and LEDs drivers.
| #define BOARD_USB2AX_V31 53 |
Selects the USB2AX version 3.1 specific board drivers, including the Button and LEDs drivers.
| #define BOARD_USBFOO 25 |
Selects the Kernel Concepts USBFOO specific board drivers, including the Button and LEDs drivers.
| #define BOARD_USBKEY 2 |
Selects the USBKEY specific board drivers, including Temperature, Button, Dataflash, Joystick and LED drivers.
| #define BOARD_USBTINYMKII 12 |
Selects the USBTINY MKII specific board drivers, including the Button and LEDs drivers.
| #define BOARD_USER 0 |
Selects the user-defined board drivers, which should be placed in the user project's folder under a directory named /Board/. Each board driver should be named identically to the LUFA master board driver (i.e., driver in the LUFA/Drivers/Board directory) so that the library can correctly identify it.
| #define BOARD_XPLAIN 8 |
Selects the XPLAIN (Revision 2 or newer) specific board drivers, including LED and Dataflash drivers.
| #define BOARD_XPLAIN_REV1 9 |
Selects the XPLAIN (Revision 1) specific board drivers, including LED and Dataflash drivers.