Digital button board hardware driver. More...
Modules | |
| A3BU_XPLAINED | |
| Board specific Buttons driver header for the Atmel XMEGA A3BU Xplained. | |
| ATAVRUSBRF01 | |
| Board specific Buttons driver header for the Atmel ATAVRUSBRF01. | |
| B1_XPLAINED | |
| Board specific Buttons driver header for the Atmel XMEGA B1 Xplained. | |
| BENITO | |
| Board specific Buttons driver header for the Tempusdictum Benito. | |
| BUMBLEB | |
| Board specific Buttons driver header for the Fletchtronics BUMBLEB. | |
| C3_XPLAINED | |
| Board specific Buttons driver header for the Atmel XMEGA C3 Xplained. | |
| CULV3 | |
| Board specific Buttons driver header for the Busware CULV3. | |
| EVK1100 | |
| Board specific Buttons driver header for the Atmel EVK1100. | |
| EVK1101 | |
| Board specific Buttons driver header for the Atmel EVK1101. | |
| EVK1104 | |
| Board specific Buttons driver header for the Atmel EVK1104. | |
| EVK527 | |
| Board specific Buttons driver header for the Atmel EVK527. | |
| JMDBU2 | |
| Board specific Buttons driver header for the Mattairtech JM-DB-U2. | |
| MICROPENDOUS_1 | |
| Board specific Button driver header for the Micropendous 1 (https://code.google.com/p/micropendous/wiki/Micropendous1). | |
| MICROPENDOUS_2 | |
| Board specific Button driver header for the Micropendous 2 (https://code.google.com/p/micropendous/wiki/Micropendous2). | |
| MICROPENDOUS_3 | |
| Board specific Button driver header for the Micropendous 3 (https://code.google.com/p/micropendous/wiki/Micropendous3). | |
| MICROPENDOUS_32U2 | |
| Board specific Buttons driver header for the Micropendous 32U2. | |
| MICROPENDOUS_4 | |
| Board specific Button driver header for the Micropendous 4 (https://code.google.com/p/micropendous/wiki/Micropendous4). | |
| MICROPENDOUS_A | |
| Board specific Button driver header for the Micropendous A (https://code.google.com/p/micropendous/wiki/MicropendousA). | |
| MICROPENDOUS_DIP | |
| Board specific Button driver header for the Micropendous DIP (https://code.google.com/p/micropendous/wiki/MicropendousDIP). | |
| MICROPENDOUS_REV1 | |
| Board specific Button driver header for the Micropendous Arduino-like Revision 1 (https://code.google.com/p/micropendous/wiki/Micropendous). | |
| MICROPENDOUS_REV2 | |
| Board specific Button driver header for the Micropendous Arduino-like Revision 2 (https://code.google.com/p/micropendous/wiki/Micropendous). | |
| MICROSIN162 | |
| Board specific Buttons driver header for the Microsin AVR-USB162 board. | |
| MINIMUS | |
| Board specific Buttons driver header for the MINIMUS. | |
| OLIMEX162 | |
| Board specific Buttons driver header for the Olimex AVR-USB-162 Development Board. | |
| OLIMEX32U4 | |
| Board specific Buttons driver header for the Olimex AVR-USB-32U4 Development Board. | |
| OLIMEXISPMK2 | |
| Board specific Buttons driver header for the Olimex AVR-ISP-MK2. | |
| OLIMEXT32U4 | |
| Board specific Buttons driver header for the Olimex AVR-USB-32U4 Development Board. | |
| STANGE_ISP | |
| Board specific Buttons driver header for the Dimex Stange-ISP. | |
| STK525 | |
| Board specific Buttons driver header for the Atmel STK525. | |
| STK526 | |
| Board specific Buttons driver header for the Atmel STK526. | |
| TUL | |
| Board specific Buttons driver header for the TUL. | |
| U2S | |
| Board specific Buttons driver header for the U2S. | |
| UC3A3_XPLAINED | |
| Board specific Buttons driver header for the Atmel UC3-A3 Xplained. | |
| UDIP | |
| Board specific Buttons driver header for the UDIP. | |
| USB2AX | |
| Board specific Buttons driver header for the Xevelabs USB2AX revisions 1 and 2. | |
| USB2AX_V3 | |
| Board specific Button driver header for the Xevelabs USB2AX revision 3. | |
| USB2AX_V31 | |
| Board specific Button driver header for the Xevelabs USB2AX revision 3.1. | |
| USBFOO | |
| Board specific Buttons driver header for the Kernel Concepts USBFOO. | |
| USBKEY | |
| Board specific Buttons driver header for the Atmel USBKEY. | |
| USBTINYMKII | |
| Board specific Buttons driver header for Tom's USBTINY MKII. | |
Functions | |
| static void | Buttons_Disable (void) |
| static uint_reg_t | Buttons_GetStatus (void) ATTR_WARN_UNUSED_RESULT |
| static void | Buttons_Init (void) |
The following files must be built with any user project that uses this module:
Hardware buttons driver. This provides an easy to use driver for the hardware buttons present on many boards. It provides a way to easily configure and check the status of all the buttons on the board so that appropriate actions can be taken.
If the BOARD value is set to BOARD_USER, this will include the /Board/Buttons.h file in the user project directory. Otherwise, it will include the appropriate built-in board driver header file.
For possible BOARD makefile values, see Board Types.
The following snippet is an example of how this module may be used within a typical application.
|
inlinestatic |
Disables the buttons driver, releasing the I/O pins back to their default high-impedance input mode.
|
inlinestatic |
Returns a mask indicating which board buttons are currently pressed.
BUTTONS_BUTTON* constants indicating which board buttons are currently pressed.
|
inlinestatic |
Initializes the buttons driver, so that the current button position can be read. This sets the appropriate I/O pins to an inputs with pull-ups enabled.
This must be called before any Button driver functions are used.