Board specific Buttons driver header for the Dimex Stange-ISP. More...
Macros | |
| #define | BUTTONS_BUTTON1 (1 << 7) |
Board specific Buttons driver header for the Dimex Stange-ISP board (http://www.diamex.de/dxshop/USB-ISP-Programmer-fuer-Atmel-AVR).
| Name | Info | Active Level | Port Pin |
|---|---|---|---|
| BUTTONS_BUTTON1 | HWB Button | Low | PORTD.7 |
| #define BUTTONS_BUTTON1 (1 << 7) |
Button mask for the first button on the board.