USB Device management definitions for USB device mode. More...
Modules | |
| Device Management (AVR8) | |
| USB Device definitions for the AVR8 microcontrollers. | |
| Device Management (EFM32GG) | |
| USB Device definitions for the EFM32 Giant Gecko microcontrollers. | |
| Device Management (UC3) | |
| USB Device definitions for the AVR32 UC3 microcontrollers. | |
| Device Management (XMEGA) | |
| USB Device definitions for the AVR XMEGA microcontrollers. | |
Enumerations | |
| enum | USB_DescriptorMemorySpaces_t { MEMSPACE_FLASH = 0, MEMSPACE_EEPROM = 1, MEMSPACE_RAM = 2 } |
| enum | USB_Device_States_t { DEVICE_STATE_Unattached = 0, DEVICE_STATE_Powered = 1, DEVICE_STATE_Default = 2, DEVICE_STATE_Addressed = 3, DEVICE_STATE_Configured = 4, DEVICE_STATE_Suspended = 5 } |
Functions | |
| uint16_t | CALLBACK_USB_GetDescriptor (const uint16_t wValue, const uint8_t wIndex, const void **const DescriptorAddress, uint8_t *const DescriptorMemorySpace) ATTR_WARN_UNUSED_RESULT ATTR_NON_NULL_PTR_ARG(3) |
Variables | |
| uint8_t | USB_Device_ConfigurationNumber |
| bool | USB_Device_CurrentlySelfPowered |
| bool | USB_Device_RemoteWakeupEnabled |
| volatile uint8_t | USB_DeviceState |
USB Device mode related definitions common to all architectures. This module contains definitions which are used when the USB controller is initialized in device mode.
Enum for the possible descriptor memory spaces, for the MemoryAddressSpace parameter of the CALLBACK_USB_GetDescriptor() function. This can be used when none of the USE_*_DESCRIPTORS compile time options are used, to indicate in which memory space the descriptor is stored.
| enum USB_Device_States_t |
Enum for the various states of the USB Device state machine. Only some states are implemented in the LUFA library - other states are left to the user to implement.
For information on each possible USB device state, refer to the USB 2.0 specification.
| uint16_t CALLBACK_USB_GetDescriptor | ( | const uint16_t | wValue, |
| const uint8_t | wIndex, | ||
| const void **const | DescriptorAddress, | ||
| uint8_t *const | DescriptorMemorySpace | ||
| ) |
Function to retrieve a given descriptor's size and memory location from the given descriptor type value, index and language ID. This function MUST be overridden in the user application (added with full, identical prototype and name so that the library can call it to retrieve descriptor data.
| [in] | wValue | The type of the descriptor to retrieve in the upper byte, and the index in the lower byte (when more than one descriptor of the given type exists, such as the case of string descriptors). The type may be one of the standard types defined in the DescriptorTypes_t enum, or may be a class-specific descriptor type value. |
| [in] | wIndex | The language ID of the string to return if the wValue type indicates DTYPE_String, otherwise zero for standard descriptors, or as defined in a class-specific standards. |
| [out] | DescriptorAddress | Pointer to the descriptor in memory. This should be set by the routine to the address of the descriptor. |
| [out] | DescriptorMemorySpace | A value from the USB_DescriptorMemorySpaces_t enum to indicate the memory space in which the descriptor is stored. This parameter does not exist when one of the USE_*_DESCRIPTORS compile time options is used, or on architectures which use a unified address space. |
PROGMEM attribute. If descriptors should be located in RAM or EEPROM instead (to speed up access in the case of RAM, or to allow the descriptors to be changed dynamically at runtime) either the USE_RAM_DESCRIPTORS or the USE_EEPROM_DESCRIPTORS tokens may be defined in the project makefile and passed to the compiler by the -D switch.| uint8_t USB_Device_ConfigurationNumber |
Indicates the currently set configuration number of the device. USB devices may have several different configurations which the host can select between; this indicates the currently selected value, or 0 if no configuration has been selected.
| bool USB_Device_CurrentlySelfPowered |
Indicates if the device is currently being powered by its own power supply, rather than being powered by the host's USB supply. This flag should remain cleared if the device does not support self powered mode, as indicated in the device descriptors.
| bool USB_Device_RemoteWakeupEnabled |
Indicates if the host is currently allowing the device to issue remote wakeup events. If this flag is cleared, the device should not issue remote wakeup events to the host.
NO_DEVICE_REMOTE_WAKEUP token in the project makefile and passing it to the compiler via the -D switch. | volatile uint8_t USB_DeviceState |
Indicates the current device state machine state. When in device mode, this indicates the state via one of the values of the USB_Device_States_t enum values.
This value should not be altered by the user application as it is handled automatically by the library. The only exception to this rule is if the NO_LIMITED_CONTROLLER_CONNECT token is used (see EVENT_USB_Device_Connect() and EVENT_USB_Device_Disconnect() events).
To reduce program size and speed up checks of this global on the AVR8 architecture, it can be placed into one of the AVR's GPIOR hardware registers instead of RAM by defining the DEVICE_STATE_AS_GPIOR token to a value between 0 and 2 in the project makefile and passing it to the compiler via the -D switch. When defined, the corresponding GPIOR register should not be used in the user application except implicitly via the library APIs.