Endpoint data read/write definitions for the Atmel AVR XMEGA architecture. More...
Functions | |
| static uint16_t | Endpoint_BytesInEndpoint (void) ATTR_WARN_UNUSED_RESULT ATTR_ALWAYS_INLINE |
| uint8_t | Endpoint_WaitUntilReady (void) |
Functions, macros, variables, enums and types related to data reading and writing from and to endpoints.
Enum for the possible error return codes of the Endpoint_WaitUntilReady() function.
| Enumerator | |
|---|---|
| ENDPOINT_READYWAIT_NoError |
Endpoint is ready for next packet, no error. |
| ENDPOINT_READYWAIT_EndpointStalled |
The endpoint was stalled during the stream transfer by the host or device. |
| ENDPOINT_READYWAIT_DeviceDisconnected |
Device was disconnected from the host while waiting for the endpoint to become ready. |
| ENDPOINT_READYWAIT_BusSuspended |
The USB bus has been suspended by the host and no USB endpoint traffic can occur until the bus has resumed. |
| ENDPOINT_READYWAIT_Timeout |
The host failed to accept or send the next packet within the software timeout period set by the USB_STREAM_TIMEOUT_MS macro. |
| ENDPOINT_READYWAIT_NoError |
Endpoint is ready for next packet, no error. |
| ENDPOINT_READYWAIT_EndpointStalled |
The endpoint was stalled during the stream transfer by the host or device. |
| ENDPOINT_READYWAIT_DeviceDisconnected |
Device was disconnected from the host while waiting for the endpoint to become ready. |
| ENDPOINT_READYWAIT_BusSuspended |
The USB bus has been suspended by the host and no USB endpoint traffic can occur until the bus has resumed. |
| ENDPOINT_READYWAIT_Timeout |
The host failed to accept or send the next packet within the software timeout period set by the USB_STREAM_TIMEOUT_MS macro. |
| ENDPOINT_READYWAIT_NoError |
Endpoint is ready for next packet, no error. |
| ENDPOINT_READYWAIT_EndpointStalled |
The endpoint was stalled during the stream transfer by the host or device. |
| ENDPOINT_READYWAIT_DeviceDisconnected |
Device was disconnected from the host while waiting for the endpoint to become ready. |
| ENDPOINT_READYWAIT_BusSuspended |
The USB bus has been suspended by the host and no USB endpoint traffic can occur until the bus has resumed. |
| ENDPOINT_READYWAIT_Timeout |
The host failed to accept or send the next packet within the software timeout period set by the USB_STREAM_TIMEOUT_MS macro. |
| ENDPOINT_READYWAIT_NoError |
Endpoint is ready for next packet, no error. |
| ENDPOINT_READYWAIT_EndpointStalled |
The endpoint was stalled during the stream transfer by the host or device. |
| ENDPOINT_READYWAIT_DeviceDisconnected |
Device was disconnected from the host while waiting for the endpoint to become ready. |
| ENDPOINT_READYWAIT_BusSuspended |
The USB bus has been suspended by the host and no USB endpoint traffic can occur until the bus has resumed. |
| ENDPOINT_READYWAIT_Timeout |
The host failed to accept or send the next packet within the software timeout period set by the USB_STREAM_TIMEOUT_MS macro. |
|
inlinestatic |
Indicates the number of bytes currently stored in the current endpoint's selected bank.
| uint8_t Endpoint_WaitUntilReady | ( | void | ) |
Spin-loops until the currently selected non-control endpoint is ready for the next packet of data to be read or written to it.