Board specific joystick driver header for the Fletchtronics BUMBLEB. More...
Macros | |
| #define | JOY_DOWN (1 << 1) |
| #define | JOY_LEFT (1 << 2) |
| #define | JOY_PRESS (1 << 4) |
| #define | JOY_RIGHT (1 << 0) |
| #define | JOY_UP (1 << 3) |
Board specific joystick driver header for the Fletchtronics BUMBLEB (http://fletchtronics.net/bumble-b). The BUMBLEB third-party board does not include any on-board peripherals, but does have an officially recommended external peripheral layout for buttons, LEDs and a Joystick.
| Left Port Pin | Up Port Pin | Right Port Pin | Down Port Pin | Press Port Pin |
|---|---|---|---|---|
| PORTD.2 | PORTD.3 | PORTD.0 | PORTD.1 | PORTD.4 |
| #define JOY_DOWN (1 << 1) |
Mask for the joystick being pushed in the downward direction.
| #define JOY_LEFT (1 << 2) |
Mask for the joystick being pushed in the left direction.
| #define JOY_PRESS (1 << 4) |
Mask for the joystick being pushed inward.
| #define JOY_RIGHT (1 << 0) |
Mask for the joystick being pushed in the right direction.
| #define JOY_UP (1 << 3) |
Mask for the joystick being pushed in the upward direction.