Board specific LED driver header for the Tempusdictum Benito. More...
Macros | |
| #define | LEDS_ALL_LEDS (LEDS_LED1 | LEDS_LED2) |
| #define | LEDS_LED1 (1 << 7) |
| #define | LEDS_LED2 (1 << 6) |
| #define | LEDS_NO_LEDS 0 |
Board specific LED driver header for the Tempusdictum Benito (http://dorkbotpdx.org/wiki/benito).
| Name | Color | Info | Active Level | Port Pin |
|---|---|---|---|---|
| LEDS_LED1 | Green | TX LED | Low | PORTC.7 |
| LEDS_LED2 | Red | RX LED | Low | PORTC.6 |
| #define LEDS_LED1 (1 << 7) |
LED mask for the first LED on the board.
| #define LEDS_LED2 (1 << 6) |
LED mask for the second LED on the board.
| #define LEDS_NO_LEDS 0 |
LED mask for none of the board LEDs.