Board specific LED driver header for the Busware BUI. More...
Macros | |
| #define | LEDS_ALL_LEDS (LEDS_LED1 | LEDS_LED2 | LEDS_LED3) |
| #define | LEDS_LED1 (1 << 2) |
| #define | LEDS_LED2 (1 << 3) |
| #define | LEDS_LED3 (1 << 4) |
| #define | LEDS_NO_LEDS 0 |
Board specific LED driver header for the Busware BUI (http://www.busware.de/tiki-index.php?page=BUI).
| Name | Color | Info | Active Level | Port Pin |
|---|---|---|---|---|
| LEDS_LED1 | Red | RGB LED | High | PORTC.2 |
| LEDS_LED2 | Green | RGB LED | High | PORTC.3 |
| LEDS_LED3 | Blue | RGB LED | High | PORTC.4 |
| #define LEDS_LED1 (1 << 2) |
LED mask for the first LED on the board.
| #define LEDS_LED2 (1 << 3) |
LED mask for the second LED on the board.
| #define LEDS_LED3 (1 << 4) |
LED mask for the third LED on the board.
| #define LEDS_NO_LEDS 0 |
LED mask for none of the board LEDs.