Board specific LED driver header for the Bitwizard Multio. More...
Macros | |
| #define | LEDS_ALL_LEDS (LEDS_LED1 | LEDS_LED2 | LEDS_LED3) |
| #define | LEDS_LED1 (1 << 0) |
| #define | LEDS_LED2 (1 << 2) |
| #define | LEDS_LED3 (1 << 7) |
| #define | LEDS_NO_LEDS 0 |
Board specific LED driver header for the Bitwizard Multio (http://www.bitwizard.nl/wiki/index.php/USB-multio).
| Name | Color | Info | Active Level | Port Pin |
|---|---|---|---|---|
| LEDS_LED1 | Green | General Indicator | High | PORTD.0 |
| LEDS_LED2 | Green | General Indicator | High | PORTC.2 |
| LEDS_LED3 | Green | General Indicator | High | PORTD.7 |
| #define LEDS_LED1 (1 << 0) |
LED mask for the first LED on the board.
| #define LEDS_LED2 (1 << 2) |
LED mask for the second LED on the board.
| #define LEDS_LED3 (1 << 7) |
LED mask for the second LED on the board.
| #define LEDS_NO_LEDS 0 |
LED mask for none of the board LEDs.