Board specific LED driver header for the Atmel RZUSBSTICK. More...
Macros | |
| #define | LEDS_ALL_LEDS (LEDS_LED1 | LEDS_LED2 | LEDS_LED3 | LEDS_LED4) |
| #define | LEDS_LED1 (1 << 7) |
| #define | LEDS_LED2 (1 << 5) |
| #define | LEDS_LED3 ((1 << 6) >> LEDS_PORTE_MASK_SHIFT) |
| #define | LEDS_LED4 ((1 << 7) >> LEDS_PORTE_MASK_SHIFT) |
| #define | LEDS_NO_LEDS 0 |
Board specific LED driver header for the Atmel RZUSBSTICK.
| Name | Color | Info | Active Level | Port Pin |
|---|---|---|---|---|
| LEDS_LED1 | Blue | General Indicator | High | PORTD.7 |
| LEDS_LED1 | Red | General Indicator | Low | PORTD.5 |
| LEDS_LED1 | Green | General Indicator | Low | PORTE.6 |
| LEDS_LED1 | Yellow | General Indicator | Low | PORTE.7 |
LED mask for all the LEDs on the board.
| #define LEDS_LED1 (1 << 7) |
LED mask for the first LED on the board.
| #define LEDS_LED2 (1 << 5) |
LED mask for the second LED on the board.
| #define LEDS_LED3 ((1 << 6) >> LEDS_PORTE_MASK_SHIFT) |
LED mask for the third LED on the board.
| #define LEDS_LED4 ((1 << 7) >> LEDS_PORTE_MASK_SHIFT) |
LED mask for the fourth LED on the board.
| #define LEDS_NO_LEDS 0 |
LED mask for none of the board LEDs.