Board specific LED driver header for the Dimex Stange-ISP board. More...
Macros | |
| #define | LEDS_ALL_LEDS (LEDS_LED1 | LEDS_LED2) |
| #define | LEDS_LED1 (1 << 0) |
| #define | LEDS_LED2 (1 << 1) |
| #define | LEDS_NO_LEDS 0 |
Board specific LED driver header for the Dimex Stange-ISP board (http://www.diamex.de/dxshop/USB-ISP-Programmer-fuer-Atmel-AVR).
| Name | Color | Info | Active Level | Port Pin |
|---|---|---|---|---|
| LEDS_LED1 | Green | General Indicator | Low | PORTD.0 |
| LEDS_LED2 | Red | General Indicator | Low | PORTD.1 |
| #define LEDS_LED1 (1 << 0) |
LED mask for the first LED on the board.
| #define LEDS_LED2 (1 << 1) |
LED mask for the second LED on the board.
| #define LEDS_NO_LEDS 0 |
LED mask for none of the board LEDs.