Board specific LED driver header for the Arduino Uno. More...
Macros | |
| #define | LEDS_ALL_LEDS (LEDS_LED1 | LEDS_LED2) |
| #define | LEDS_LED1 (1 << 4) |
| #define | LEDS_LED2 (1 << 5) |
| #define | LEDS_NO_LEDS 0 |
Board specific LED driver header for the Arduino Uno (http://arduino.cc/en/Main/ArduinoBoardUno).
| Name | Color | Info | Active Level | Port Pin |
|---|---|---|---|---|
| LEDS_LED1 | Yellow | RX | Low | PORTD.4 |
| LEDS_LED2 | Yellow | TX | Low | PORTD.5 |
| #define LEDS_LED1 (1 << 4) |
LED mask for the first LED on the board.
| #define LEDS_LED2 (1 << 5) |
LED mask for the second LED on the board.
| #define LEDS_NO_LEDS 0 |
LED mask for none of the board LEDs.