Pipe management definitions.
More...
This module contains functions, macros and enums related to pipe management when in USB Host mode. This module contains the pipe management macros, as well as pipe interrupt and data send/receive functions for various data types.
| #define PIPE_CONTROLPIPE 0 |
Pipe address for the default control pipe, which always resides in address 0. This is defined for convenience to give more readable code when used with the pipe macros.
| #define PIPE_EPNUM_MASK 0x0F |
Endpoint number mask, for masking against endpoint addresses to retrieve the endpoint's numerical address in the attached device.
| #define PIPE_PIPENUM_MASK 0x0F |
Pipe number mask, for masking against pipe addresses to retrieve the pipe's numerical address in the device.