Pipe data stream transmission and reception management. More...
Modules | |
| Read/Write of Multi-Byte Streams (AVR8) | |
| Pipe data stream transmission and reception management for the Atmel AVR8 architecture. | |
| Read/Write of Multi-Byte Streams (UC3) | |
| Pipe data stream transmission and reception management for the Atmel AVR32 UC3 architecture. | |
Enumerations | |
| enum | Pipe_Stream_RW_ErrorCodes_t { PIPE_RWSTREAM_NoError = 0, PIPE_RWSTREAM_PipeStalled = 1, PIPE_RWSTREAM_DeviceDisconnected = 2, PIPE_RWSTREAM_Timeout = 3, PIPE_RWSTREAM_IncompleteTransfer = 4 } |
Functions, macros, variables, enums and types related to data reading and writing of data streams from and to pipes.
Enum for the possible error return codes of the Pipe_*_Stream_* functions.
| Enumerator | |
|---|---|
| PIPE_RWSTREAM_NoError |
Command completed successfully, no error. |
| PIPE_RWSTREAM_PipeStalled |
The device stalled the pipe during the transfer. |
| PIPE_RWSTREAM_DeviceDisconnected |
Device was disconnected from the host during the transfer. |
| PIPE_RWSTREAM_Timeout |
The device failed to accept or send the next packet within the software timeout period set by the USB_STREAM_TIMEOUT_MS macro. |
| PIPE_RWSTREAM_IncompleteTransfer |
Indicates that the pipe bank became full/empty before the complete contents of the stream could be transferred. |