USB control endpoint request definitions. More...
Data Structures | |
| struct | USB_Request_Header_t |
| Standard USB Control Request. More... | |
Macros | |
| #define | CONTROL_REQTYPE_DIRECTION 0x80 |
| #define | CONTROL_REQTYPE_RECIPIENT 0x1F |
| #define | CONTROL_REQTYPE_TYPE 0x60 |
Enumerations | |
| enum | USB_Control_Request_t { REQ_GetStatus = 0, REQ_ClearFeature = 1, REQ_SetFeature = 3, REQ_SetAddress = 5, REQ_GetDescriptor = 6, REQ_SetDescriptor = 7, REQ_GetConfiguration = 8, REQ_SetConfiguration = 9, REQ_GetInterface = 10, REQ_SetInterface = 11, REQ_SynchFrame = 12 } |
| enum | USB_Feature_Selectors_t { FEATURE_SEL_EndpointHalt = 0x00, FEATURE_SEL_DeviceRemoteWakeup = 0x01, FEATURE_SEL_TestMode = 0x02 } |
Control Request Data Direction Masks | |
| #define | REQDIR_HOSTTODEVICE (0 << 7) |
| #define | REQDIR_DEVICETOHOST (1 << 7) |
Control Request Type Masks | |
| #define | REQTYPE_STANDARD (0 << 5) |
| #define | REQTYPE_CLASS (1 << 5) |
| #define | REQTYPE_VENDOR (2 << 5) |
Control Request Recipient Masks | |
| #define | REQREC_DEVICE (0 << 0) |
| #define | REQREC_INTERFACE (1 << 0) |
| #define | REQREC_ENDPOINT (2 << 0) |
| #define | REQREC_OTHER (3 << 0) |
This module contains definitions for the various control request parameters, so that the request details (such as data direction, request recipient, etc.) can be extracted via masking.
| #define CONTROL_REQTYPE_DIRECTION 0x80 |
Mask for the request type parameter, to indicate the direction of the request data (Host to Device or Device to Host). The result of this mask should then be compared to the request direction masks.
REQDIR_* macros for masks indicating the request data direction. | #define CONTROL_REQTYPE_RECIPIENT 0x1F |
Mask for the request type parameter, to indicate the recipient of the request (Device, Interface Endpoint or Other). The result of this mask should then be compared to the request recipient masks.
REQREC_* macros for masks indicating the request recipient. | #define CONTROL_REQTYPE_TYPE 0x60 |
Mask for the request type parameter, to indicate the type of request (Device, Class or Vendor Specific). The result of this mask should then be compared to the request type masks.
REQTYPE_* macros for masks indicating the request type. | #define REQDIR_DEVICETOHOST (1 << 7) |
Request data direction mask, indicating that the request data will flow from device to host.
| #define REQDIR_HOSTTODEVICE (0 << 7) |
Request data direction mask, indicating that the request data will flow from host to device.
| #define REQREC_DEVICE (0 << 0) |
Request recipient mask, indicating that the request is to be issued to the device as a whole.
| #define REQREC_ENDPOINT (2 << 0) |
Request recipient mask, indicating that the request is to be issued to an endpoint in the currently selected configuration.
| #define REQREC_INTERFACE (1 << 0) |
Request recipient mask, indicating that the request is to be issued to an interface in the currently selected configuration.
| #define REQREC_OTHER (3 << 0) |
Request recipient mask, indicating that the request is to be issued to an unspecified element in the currently selected configuration.
| #define REQTYPE_CLASS (1 << 5) |
Request type mask, indicating that the request is a class-specific request.
| #define REQTYPE_STANDARD (0 << 5) |
Request type mask, indicating that the request is a standard request.
| #define REQTYPE_VENDOR (2 << 5) |
Request type mask, indicating that the request is a vendor specific request.
Enumeration for the various standard request commands. These commands are applicable when the request type is REQTYPE_STANDARD (with the exception of REQ_GetDescriptor, which is always handled regardless of the request type value).
| Enumerator | |
|---|---|
| REQ_GetStatus |
Implemented in the library for device and endpoint recipients. Passed to the user application for other recipients via the EVENT_USB_Device_ControlRequest() event when received in device mode. |
| REQ_ClearFeature |
Implemented in the library for device and endpoint recipients. Passed to the user application for other recipients via the EVENT_USB_Device_ControlRequest() event when received in device mode. |
| REQ_SetFeature |
Implemented in the library for device and endpoint recipients. Passed to the user application for other recipients via the EVENT_USB_Device_ControlRequest() event when received in device mode. |
| REQ_SetAddress |
Implemented in the library for the device recipient. Passed to the user application for other recipients via the EVENT_USB_Device_ControlRequest() event when received in device mode. |
| REQ_GetDescriptor |
Implemented in the library for device and interface recipients. Passed to the user application for other recipients via the EVENT_USB_Device_ControlRequest() event when received in device mode. |
| REQ_SetDescriptor |
Not implemented in the library, passed to the user application via the EVENT_USB_Device_ControlRequest() event when received in device mode. |
| REQ_GetConfiguration |
Implemented in the library for the device recipient. Passed to the user application for other recipients via the EVENT_USB_Device_ControlRequest() event when received in device mode. |
| REQ_SetConfiguration |
Implemented in the library for the device recipient. Passed to the user application for other recipients via the EVENT_USB_Device_ControlRequest() event when received in device mode. |
| REQ_GetInterface |
Not implemented in the library, passed to the user application via the EVENT_USB_Device_ControlRequest() event when received in device mode. |
| REQ_SetInterface |
Not implemented in the library, passed to the user application via the EVENT_USB_Device_ControlRequest() event when received in device mode. |
| REQ_SynchFrame |
Not implemented in the library, passed to the user application via the EVENT_USB_Device_ControlRequest() event when received in device mode. |
Feature Selector values for Set Feature and Clear Feature standard control requests directed to the device, interface and endpoint recipients.