USB class driver for the Google Android Open Accessory class standard. More...
Modules | |
| Android Open Accessory Class Host Mode Driver | |
| Common Class Definitions | |
The following files must be built with any user project that uses this module:
Android Open Accessory Class Driver module. This module contains an internal implementation of the USB Android Open Accessory Class, for Host USB mode. User applications can use this class driver instead of implementing the Android Open Accessory Class manually via the low-level LUFA APIs.
This module is designed to simplify the user code by exposing only the required interface needed to interface with Host using the USB Android Open Accessory Class.