USB class driver for the USB-IF Audio 1.0 class standard. More...
Modules | |
| Audio 1.0 Class Device Mode Driver | |
| Audio 1.0 Class Host Mode Driver | |
| Common Class Definitions | |
The following files must be built with any user project that uses this module:
Audio 1.0 Class Driver module. This module contains an internal implementation of the USB Audio 1.0 Class, for both Device and Host USB modes. User applications can use this class driver instead of implementing the Audio 1.0 class manually via the low-level LUFA APIs.
This module is designed to simplify the user code by exposing only the required interface needed to interface with Hosts or Devices using the USB Audio 1.0 Class.