|
| bool | Audio_Device_ConfigureEndpoints (USB_ClassInfo_Audio_Device_t *const AudioInterfaceInfo) ATTR_NON_NULL_PTR_ARG(1) |
| |
| static bool | Audio_Device_IsReadyForNextSample (USB_ClassInfo_Audio_Device_t *const AudioInterfaceInfo) ATTR_NON_NULL_PTR_ARG(1) ATTR_ALWAYS_INLINE |
| |
| static bool | Audio_Device_IsSampleReceived (USB_ClassInfo_Audio_Device_t *const AudioInterfaceInfo) ATTR_NON_NULL_PTR_ARG(1) ATTR_ALWAYS_INLINE |
| |
| void | Audio_Device_ProcessControlRequest (USB_ClassInfo_Audio_Device_t *const AudioInterfaceInfo) ATTR_NON_NULL_PTR_ARG(1) |
| |
| static int16_t | Audio_Device_ReadSample16 (USB_ClassInfo_Audio_Device_t *const AudioInterfaceInfo) ATTR_NON_NULL_PTR_ARG(1) ATTR_ALWAYS_INLINE |
| |
| static int32_t | Audio_Device_ReadSample24 (USB_ClassInfo_Audio_Device_t *const AudioInterfaceInfo) ATTR_NON_NULL_PTR_ARG(1) ATTR_ALWAYS_INLINE |
| |
| static int8_t | Audio_Device_ReadSample8 (USB_ClassInfo_Audio_Device_t *const AudioInterfaceInfo) ATTR_NON_NULL_PTR_ARG(1) ATTR_ALWAYS_INLINE |
| |
| static void | Audio_Device_USBTask (USB_ClassInfo_Audio_Device_t *const AudioInterfaceInfo) ATTR_NON_NULL_PTR_ARG(1) ATTR_ALWAYS_INLINE |
| |
| static void | Audio_Device_WriteSample16 (USB_ClassInfo_Audio_Device_t *const AudioInterfaceInfo, const int16_t Sample) ATTR_NON_NULL_PTR_ARG(1) ATTR_ALWAYS_INLINE |
| |
| static void | Audio_Device_WriteSample24 (USB_ClassInfo_Audio_Device_t *const AudioInterfaceInfo, const int32_t Sample) ATTR_NON_NULL_PTR_ARG(1) ATTR_ALWAYS_INLINE |
| |
| static void | Audio_Device_WriteSample8 (USB_ClassInfo_Audio_Device_t *const AudioInterfaceInfo, const int8_t Sample) ATTR_NON_NULL_PTR_ARG(1) ATTR_ALWAYS_INLINE |
| |
| bool | CALLBACK_Audio_Device_GetSetEndpointProperty (USB_ClassInfo_Audio_Device_t *const AudioInterfaceInfo, const uint8_t EndpointProperty, const uint8_t EndpointAddress, const uint8_t EndpointControl, uint16_t *const DataLength, uint8_t *Data) ATTR_NON_NULL_PTR_ARG(1) |
| |
| bool | CALLBACK_Audio_Device_GetSetInterfaceProperty (USB_ClassInfo_Audio_Device_t *const AudioInterfaceInfo, const uint8_t Property, const uint8_t EntityAddress, const uint16_t Parameter, uint16_t *const DataLength, uint8_t *Data) ATTR_NON_NULL_PTR_ARG(1) |
| |
| void | EVENT_Audio_Device_StreamStartStop (USB_ClassInfo_Audio_Device_t *const AudioInterfaceInfo) |
| |
Module Source Dependencies
The following files must be built with any user project that uses this module:
- LUFA/Drivers/USB/Class/Device/AudioClassDevice.c (Makefile source module name: LUFA_SRC_USBCLASS)
Module Description
Device Mode USB Class driver framework interface, for the Audio 1.0 USB Class driver.
Configures the endpoints of a given Audio interface, ready for use. This should be linked to the library EVENT_USB_Device_ConfigurationChanged() event so that the endpoints are configured when the configuration containing the given Audio interface is selected.
- Parameters
-
| [in,out] | AudioInterfaceInfo | Pointer to a structure containing an Audio Class configuration and state. |
- Returns
- Boolean
true if the endpoints were successfully configured, false otherwise.
Determines if the given audio interface is ready to accept the next sample to be written to it, and selects the streaming IN endpoint ready for writing.
- Precondition
- This function must only be called when the Device state machine is in the DEVICE_STATE_Configured state or the call will fail.
- Parameters
-
| [in,out] | AudioInterfaceInfo | Pointer to a structure containing an Audio Class configuration and state. |
- Returns
- Boolean
true if the given Audio interface is ready to accept the next sample, false otherwise.
Determines if the given audio interface is ready for a sample to be read from it, and selects the streaming OUT endpoint ready for reading.
- Precondition
- This function must only be called when the Device state machine is in the DEVICE_STATE_Configured state or the call will fail.
- Parameters
-
| [in,out] | AudioInterfaceInfo | Pointer to a structure containing an Audio Class configuration and state. |
- Returns
- Boolean
true if the given Audio interface has a sample to be read, false otherwise.
Processes incoming control requests from the host, that are directed to the given Audio class interface. This should be linked to the library EVENT_USB_Device_ControlRequest() event.
- Parameters
-
| [in,out] | AudioInterfaceInfo | Pointer to a structure containing an Audio Class configuration and state. |
Reads the next 16-bit audio sample from the current audio interface.
- Precondition
- This should be preceded immediately by a call to the Audio_Device_IsSampleReceived() function to ensure that the correct endpoint is selected and ready for data.
- Parameters
-
| [in,out] | AudioInterfaceInfo | Pointer to a structure containing an Audio Class configuration and state. |
- Returns
- Signed 16-bit audio sample from the audio interface.
Reads the next 24-bit audio sample from the current audio interface.
- Precondition
- This should be preceded immediately by a call to the Audio_Device_IsSampleReceived() function to ensure that the correct endpoint is selected and ready for data.
- Parameters
-
| [in,out] | AudioInterfaceInfo | Pointer to a structure containing an Audio Class configuration and state. |
- Returns
- Signed 24-bit audio sample from the audio interface.
Reads the next 8-bit audio sample from the current audio interface.
- Precondition
- This should be preceded immediately by a call to the Audio_Device_IsSampleReceived() function to ensure that the correct endpoint is selected and ready for data.
- Parameters
-
| [in,out] | AudioInterfaceInfo | Pointer to a structure containing an Audio Class configuration and state. |
- Returns
- Signed 8-bit audio sample from the audio interface.
General management task for a given Audio class interface, required for the correct operation of the interface. This should be called frequently in the main program loop, before the master USB management task USB_USBTask().
- Parameters
-
| [in,out] | AudioInterfaceInfo | Pointer to a structure containing an Audio Class configuration and state. |
Writes the next 16-bit audio sample to the current audio interface.
- Precondition
- This should be preceded immediately by a call to the Audio_Device_IsReadyForNextSample() function to ensure that the correct endpoint is selected and ready for data.
- Parameters
-
| [in,out] | AudioInterfaceInfo | Pointer to a structure containing an Audio Class configuration and state. |
| [in] | Sample | Signed 16-bit audio sample. |
Writes the next 24-bit audio sample to the current audio interface.
- Precondition
- This should be preceded immediately by a call to the Audio_Device_IsReadyForNextSample() function to ensure that the correct endpoint is selected and ready for data.
- Parameters
-
| [in,out] | AudioInterfaceInfo | Pointer to a structure containing an Audio Class configuration and state. |
| [in] | Sample | Signed 24-bit audio sample. |
Writes the next 8-bit audio sample to the current audio interface.
- Precondition
- This should be preceded immediately by a call to the Audio_Device_IsReadyForNextSample() function to ensure that the correct endpoint is selected and ready for data.
- Parameters
-
| [in,out] | AudioInterfaceInfo | Pointer to a structure containing an Audio Class configuration and state. |
| [in] | Sample | Signed 8-bit audio sample. |
| bool CALLBACK_Audio_Device_GetSetEndpointProperty |
( |
USB_ClassInfo_Audio_Device_t *const |
AudioInterfaceInfo, |
|
|
const uint8_t |
EndpointProperty, |
|
|
const uint8_t |
EndpointAddress, |
|
|
const uint8_t |
EndpointControl, |
|
|
uint16_t *const |
DataLength, |
|
|
uint8_t * |
Data |
|
) |
| |
Audio class driver callback for the setting and retrieval of streaming endpoint properties. This callback must be implemented in the user application to handle property manipulations on streaming audio endpoints.
When the DataLength parameter is NULL, this callback should only indicate whether the specified operation is valid for the given endpoint index, and should return as fast as possible. When non-NULL, this value may be altered for GET operations to indicate the size of the retrieved data.
- Note
- The length of the retrieved data stored into the Data buffer on GET operations should not exceed the initial value of the
DataLength parameter.
- Parameters
-
| [in,out] | AudioInterfaceInfo | Pointer to a structure containing an Audio Class configuration and state. |
| [in] | EndpointProperty | Property of the endpoint to get or set, a value from Audio_ClassRequests_t. |
| [in] | EndpointAddress | Address of the streaming endpoint whose property is being referenced. |
| [in] | EndpointControl | Parameter of the endpoint to get or set, a value from Audio_EndpointControls_t. |
| [in,out] | DataLength | For SET operations, the length of the parameter data to set. For GET operations, the maximum length of the retrieved data. When NULL, the function should return whether the given property and parameter is valid for the requested endpoint without reading or modifying the Data buffer. |
| [in,out] | Data | Pointer to a location where the parameter data is stored for SET operations, or where the retrieved data is to be stored for GET operations. |
- Returns
- Boolean
true if the property GET/SET was successful, false otherwise
| bool CALLBACK_Audio_Device_GetSetInterfaceProperty |
( |
USB_ClassInfo_Audio_Device_t *const |
AudioInterfaceInfo, |
|
|
const uint8_t |
Property, |
|
|
const uint8_t |
EntityAddress, |
|
|
const uint16_t |
Parameter, |
|
|
uint16_t *const |
DataLength, |
|
|
uint8_t * |
Data |
|
) |
| |
Audio class driver callback for the setting and retrieval of streaming interface properties. This callback must be implemented in the user application to handle property manipulations on streaming audio interfaces.
When the DataLength parameter is NULL, this callback should only indicate whether the specified operation is valid for the given entity and should return as fast as possible. When non-NULL, this value may be altered for GET operations to indicate the size of the retrieved data.
- Note
- The length of the retrieved data stored into the Data buffer on GET operations should not exceed the initial value of the
DataLength parameter.
- Parameters
-
| [in,out] | AudioInterfaceInfo | Pointer to a structure containing an Audio Class configuration and state. |
| [in] | Property | Property of the interface to get or set, a value from Audio_ClassRequests_t. |
| [in] | EntityAddress | Address of the audio entity whose property is being referenced. |
| [in] | Parameter | Parameter of the entity to get or set, specific to each type of entity (see USB Audio specification). |
| [in,out] | DataLength | For SET operations, the length of the parameter data to set. For GET operations, the maximum length of the retrieved data. When NULL, the function should return whether the given property and parameter is valid for the requested endpoint without reading or modifying the Data buffer. |
| [in,out] | Data | Pointer to a location where the parameter data is stored for SET operations, or where the retrieved data is to be stored for GET operations. |
- Returns
- Boolean
true if the property GET/SET was successful, false otherwise
Audio class driver event for an Audio Stream start/stop change. This event fires each time the device receives a stream enable or disable control request from the host, to start and stop the audio stream. The current state of the stream can be determined by the State.InterfaceEnabled value inside the Audio interface structure passed as a parameter.
- Parameters
-
| [in,out] | AudioInterfaceInfo | Pointer to a structure containing an Audio Class configuration and state. |