USB class driver for the USB-IF CDC-ACM (Virtual Serial) class standard. More...
Modules | |
| CDC Class Device Mode Driver | |
| CDC Class Host Mode Driver | |
| Common Class Definitions | |
The following files must be built with any user project that uses this module:
CDC Class Driver module. This module contains an internal implementation of the USB CDC-ACM class Virtual Serial Ports, for both Device and Host USB modes. User applications can use this class driver instead of implementing the CDC class manually via the low-level LUFA APIs.
This module is designed to simplify the user code by exposing only the required interface needed to interface with Hosts or Devices using the USB CDC Class.