USB class driver for the USB-IF Human Interface Device (HID) class standard. More...
Modules | |
| Common Class Definitions | |
| HID Class Device Mode Driver | |
| HID Class Host Mode Driver | |
The following files must be built with any user project that uses this module:
HID Class Driver module. This module contains an internal implementation of the USB HID Class, for both Device and Host USB modes. User applications can use this class driver instead of implementing the HID class manually via the low-level LUFA APIs.
This module is designed to simplify the user code by exposing only the required interface needed to interface with Hosts or Devices using the USB HID Class.