Data Structures | |
| struct | USB_HID_Descriptor_HID_t |
| HID class-specific HID Descriptor (LUFA naming conventions). More... | |
| struct | USB_HID_StdDescriptor_HID_t |
| HID class-specific HID Descriptor (USB-IF naming conventions). More... | |
| struct | USB_KeyboardReport_Data_t |
| Standard HID Boot Protocol Keyboard Report. More... | |
| struct | USB_MouseReport_Data_t |
| Standard HID Boot Protocol Mouse Report. More... | |
Typedefs | |
| typedef uint8_t | USB_Descriptor_HIDReport_Datatype_t |
Enumerations | |
| enum | HID_ClassRequests_t { HID_REQ_GetReport = 0x01, HID_REQ_GetIdle = 0x02, HID_REQ_GetProtocol = 0x03, HID_REQ_SetReport = 0x09, HID_REQ_SetIdle = 0x0A, HID_REQ_SetProtocol = 0x0B } |
| enum | HID_Descriptor_ClassSubclassProtocol_t { HID_CSCP_HIDClass = 0x03, HID_CSCP_NonBootSubclass = 0x00, HID_CSCP_BootSubclass = 0x01, HID_CSCP_NonBootProtocol = 0x00, HID_CSCP_KeyboardBootProtocol = 0x01, HID_CSCP_MouseBootProtocol = 0x02 } |
| enum | HID_DescriptorTypes_t { HID_DTYPE_HID = 0x21, HID_DTYPE_Report = 0x22 } |
| enum | HID_ReportItemTypes_t { HID_REPORT_ITEM_In = 0, HID_REPORT_ITEM_Out = 1, HID_REPORT_ITEM_Feature = 2 } |
Keyboard Standard Report Modifier Masks | |
| #define | HID_KEYBOARD_MODIFIER_LEFTCTRL (1 << 0) |
| #define | HID_KEYBOARD_MODIFIER_LEFTSHIFT (1 << 1) |
| #define | HID_KEYBOARD_MODIFIER_LEFTALT (1 << 2) |
| #define | HID_KEYBOARD_MODIFIER_LEFTGUI (1 << 3) |
| #define | HID_KEYBOARD_MODIFIER_RIGHTCTRL (1 << 4) |
| #define | HID_KEYBOARD_MODIFIER_RIGHTSHIFT (1 << 5) |
| #define | HID_KEYBOARD_MODIFIER_RIGHTALT (1 << 6) |
| #define | HID_KEYBOARD_MODIFIER_RIGHTGUI (1 << 7) |
Keyboard Standard Report LED Masks | |
| #define | HID_KEYBOARD_LED_NUMLOCK (1 << 0) |
| #define | HID_KEYBOARD_LED_CAPSLOCK (1 << 1) |
| #define | HID_KEYBOARD_LED_SCROLLLOCK (1 << 2) |
| #define | HID_KEYBOARD_LED_COMPOSE (1 << 3) |
| #define | HID_KEYBOARD_LED_KANA (1 << 4) |
Common HID Device Report Descriptors | |
| #define | HID_DESCRIPTOR_JOYSTICK(MinAxisVal, MaxAxisVal, MinPhysicalVal, MaxPhysicalVal, Buttons) |
| #define | HID_DESCRIPTOR_KEYBOARD(MaxKeys) |
| #define | HID_DESCRIPTOR_MOUSE(MinAxisVal, MaxAxisVal, MinPhysicalVal, MaxPhysicalVal, Buttons, AbsoluteCoords) |
| #define | HID_DESCRIPTOR_VENDOR(VendorPageNum, CollectionUsage, DataINUsage, DataOUTUsage, NumBytes) |
Constants, Types and Enum definitions that are common to both Device and Host modes for the USB HID Class.
| #define HID_DESCRIPTOR_JOYSTICK | ( | MinAxisVal, | |
| MaxAxisVal, | |||
| MinPhysicalVal, | |||
| MaxPhysicalVal, | |||
| Buttons | |||
| ) |
A list of HID report item array elements that describe a typical HID USB Joystick. The resulting report descriptor is structured according to the following layout:
Where uintA_t is a type large enough to hold the ranges of the signed MinAxisVal and MaxAxisVal values, and intB_t is a type large enough to hold one bit per button.
| [in] | MinAxisVal | Minimum logical axis value (16-bit). |
| [in] | MaxAxisVal | Maximum logical axis value (16-bit). |
| [in] | MinPhysicalVal | Minimum physical axis value, for movement resolution calculations (16-bit). |
| [in] | MaxPhysicalVal | Maximum physical axis value, for movement resolution calculations (16-bit). |
| [in] | Buttons | Total number of buttons in the device (8-bit). |
| #define HID_DESCRIPTOR_KEYBOARD | ( | MaxKeys | ) |
A list of HID report item array elements that describe a typical HID USB keyboard. The resulting report descriptor is compatible with USB_KeyboardReport_Data_t when MaxKeys is equal to 6. For other values, the report will be structured according to the following layout:
| [in] | MaxKeys | Number of simultaneous keys that can be reported at the one time (8-bit). |
| #define HID_DESCRIPTOR_MOUSE | ( | MinAxisVal, | |
| MaxAxisVal, | |||
| MinPhysicalVal, | |||
| MaxPhysicalVal, | |||
| Buttons, | |||
| AbsoluteCoords | |||
| ) |
A list of HID report item array elements that describe a typical HID USB mouse. The resulting report descriptor is compatible with USB_MouseReport_Data_t if the MinAxisVal and MaxAxisVal values fit within a int8_t range and the number of Buttons is less than 8. For other values, the report is structured according to the following layout:
Where intA_t is a type large enough to hold one bit per button, and intB_t is a type large enough to hold the ranges of the signed MinAxisVal and MaxAxisVal values.
| [in] | MinAxisVal | Minimum X/Y logical axis value (16-bit). |
| [in] | MaxAxisVal | Maximum X/Y logical axis value (16-bit). |
| [in] | MinPhysicalVal | Minimum X/Y physical axis value, for movement resolution calculations (16-bit). |
| [in] | MaxPhysicalVal | Maximum X/Y physical axis value, for movement resolution calculations (16-bit). |
| [in] | Buttons | Total number of buttons in the device (8-bit). |
| [in] | AbsoluteCoords | Boolean true to use absolute X/Y coordinates (e.g. touchscreen). |
| #define HID_DESCRIPTOR_VENDOR | ( | VendorPageNum, | |
| CollectionUsage, | |||
| DataINUsage, | |||
| DataOUTUsage, | |||
| NumBytes | |||
| ) |
A list of HID report item array elements that describe a typical Vendor Defined byte array HID report descriptor, used for transporting arbitrary data between the USB host and device via HID reports. The resulting report should be a uint8_t byte array of the specified length in both Device to Host (IN) and Host to Device (OUT) directions.
| [in] | VendorPageNum | Vendor Defined HID Usage Page index, ranging from 0x00 to 0xFF. |
| [in] | CollectionUsage | Vendor Usage for the encompassing report IN and OUT collection, ranging from 0x00 to 0xFF. |
| [in] | DataINUsage | Vendor Usage for the IN report data, ranging from 0x00 to 0xFF. |
| [in] | DataOUTUsage | Vendor Usage for the OUT report data, ranging from 0x00 to 0xFF. |
| [in] | NumBytes | Length of the data IN and OUT reports. |
| #define HID_KEYBOARD_LED_CAPSLOCK (1 << 1) |
Constant for a keyboard output report LED byte, indicating that the host's CAPS LOCK mode is currently set.
| #define HID_KEYBOARD_LED_COMPOSE (1 << 3) |
Constant for a keyboard output report LED byte, indicating that the host's COMPOSE mode is currently set.
| #define HID_KEYBOARD_LED_KANA (1 << 4) |
Constant for a keyboard output report LED byte, indicating that the host's KANA mode is currently set.
| #define HID_KEYBOARD_LED_NUMLOCK (1 << 0) |
Constant for a keyboard output report LED byte, indicating that the host's NUM LOCK mode is currently set.
| #define HID_KEYBOARD_LED_SCROLLLOCK (1 << 2) |
Constant for a keyboard output report LED byte, indicating that the host's SCROLL LOCK mode is currently set.
| #define HID_KEYBOARD_MODIFIER_LEFTALT (1 << 2) |
Constant for a keyboard report modifier byte, indicating that the keyboard's left alt key is currently pressed.
| #define HID_KEYBOARD_MODIFIER_LEFTCTRL (1 << 0) |
Constant for a keyboard report modifier byte, indicating that the keyboard's left control key is currently pressed.
| #define HID_KEYBOARD_MODIFIER_LEFTGUI (1 << 3) |
Constant for a keyboard report modifier byte, indicating that the keyboard's left GUI key is currently pressed.
| #define HID_KEYBOARD_MODIFIER_LEFTSHIFT (1 << 1) |
Constant for a keyboard report modifier byte, indicating that the keyboard's left shift key is currently pressed.
| #define HID_KEYBOARD_MODIFIER_RIGHTALT (1 << 6) |
Constant for a keyboard report modifier byte, indicating that the keyboard's right alt key is currently pressed.
| #define HID_KEYBOARD_MODIFIER_RIGHTCTRL (1 << 4) |
Constant for a keyboard report modifier byte, indicating that the keyboard's right control key is currently pressed.
| #define HID_KEYBOARD_MODIFIER_RIGHTGUI (1 << 7) |
Constant for a keyboard report modifier byte, indicating that the keyboard's right GUI key is currently pressed.
| #define HID_KEYBOARD_MODIFIER_RIGHTSHIFT (1 << 5) |
Constant for a keyboard report modifier byte, indicating that the keyboard's right shift key is currently pressed.
| #define HID_KEYBOARD_SC_0_AND_CLOSING_PARENTHESIS 0x27 |
| #define HID_KEYBOARD_SC_1_AND_EXCLAMATION 0x1E |
| #define HID_KEYBOARD_SC_2_AND_AT 0x1F |
| #define HID_KEYBOARD_SC_3_AND_HASHMARK 0x20 |
| #define HID_KEYBOARD_SC_4_AND_DOLLAR 0x21 |
| #define HID_KEYBOARD_SC_5_AND_PERCENTAGE 0x22 |
| #define HID_KEYBOARD_SC_6_AND_CARET 0x23 |
| #define HID_KEYBOARD_SC_7_AND_AND_AMPERSAND 0x24 |
| #define HID_KEYBOARD_SC_8_AND_ASTERISK 0x25 |
| #define HID_KEYBOARD_SC_9_AND_OPENING_PARENTHESIS 0x26 |
| #define HID_KEYBOARD_SC_A 0x04 |
| #define HID_KEYBOARD_SC_AGAIN 0x79 |
| #define HID_KEYBOARD_SC_ALTERNATE_ERASE 0x99 |
| #define HID_KEYBOARD_SC_APOSTROPHE_AND_QUOTE 0x34 |
| #define HID_KEYBOARD_SC_APPLICATION 0x65 |
| #define HID_KEYBOARD_SC_B 0x05 |
| #define HID_KEYBOARD_SC_BACKSLASH_AND_PIPE 0x31 |
| #define HID_KEYBOARD_SC_BACKSPACE 0x2A |
| #define HID_KEYBOARD_SC_C 0x06 |
| #define HID_KEYBOARD_SC_CANCEL 0x9B |
| #define HID_KEYBOARD_SC_CAPS_LOCK 0x39 |
| #define HID_KEYBOARD_SC_CLEAR 0x9C |
| #define HID_KEYBOARD_SC_CLEAR_AND_AGAIN 0xA2 |
| #define HID_KEYBOARD_SC_CLOSING_BRACKET_AND_CLOSING_BRACE 0x30 |
| #define HID_KEYBOARD_SC_COMMA_AND_LESS_THAN_SIGN 0x36 |
| #define HID_KEYBOARD_SC_COPY 0x7C |
| #define HID_KEYBOARD_SC_CRSEL_ANDPROPS 0xA3 |
| #define HID_KEYBOARD_SC_CURRENCY_SUB_UNIT 0xB5 |
| #define HID_KEYBOARD_SC_CURRENCY_UNIT 0xB4 |
| #define HID_KEYBOARD_SC_CUT 0x7B |
| #define HID_KEYBOARD_SC_D 0x07 |
| #define HID_KEYBOARD_SC_DECIMAL_SEPARATOR 0xB3 |
| #define HID_KEYBOARD_SC_DELETE 0x4C |
| #define HID_KEYBOARD_SC_DOT_AND_GREATER_THAN_SIGN 0x37 |
| #define HID_KEYBOARD_SC_DOWN_ARROW 0x51 |
| #define HID_KEYBOARD_SC_E 0x08 |
| #define HID_KEYBOARD_SC_END 0x4D |
| #define HID_KEYBOARD_SC_ENTER 0x28 |
| #define HID_KEYBOARD_SC_EQUAL_AND_PLUS 0x2E |
| #define HID_KEYBOARD_SC_ERROR_ROLLOVER 0x01 |
| #define HID_KEYBOARD_SC_ERROR_UNDEFINED 0x03 |
| #define HID_KEYBOARD_SC_ESCAPE 0x29 |
| #define HID_KEYBOARD_SC_EXECUTE 0x74 |
| #define HID_KEYBOARD_SC_EXSEL 0xA4 |
| #define HID_KEYBOARD_SC_F 0x09 |
| #define HID_KEYBOARD_SC_F1 0x3A |
| #define HID_KEYBOARD_SC_F10 0x43 |
| #define HID_KEYBOARD_SC_F11 0x44 |
| #define HID_KEYBOARD_SC_F12 0x45 |
| #define HID_KEYBOARD_SC_F13 0x68 |
| #define HID_KEYBOARD_SC_F14 0x69 |
| #define HID_KEYBOARD_SC_F15 0x6A |
| #define HID_KEYBOARD_SC_F16 0x6B |
| #define HID_KEYBOARD_SC_F17 0x6C |
| #define HID_KEYBOARD_SC_F18 0x6D |
| #define HID_KEYBOARD_SC_F19 0x6E |
| #define HID_KEYBOARD_SC_F2 0x3B |
| #define HID_KEYBOARD_SC_F20 0x6F |
| #define HID_KEYBOARD_SC_F21 0x70 |
| #define HID_KEYBOARD_SC_F22 0x71 |
| #define HID_KEYBOARD_SC_F23 0x72 |
| #define HID_KEYBOARD_SC_F24 0x73 |
| #define HID_KEYBOARD_SC_F3 0x3C |
| #define HID_KEYBOARD_SC_F4 0x3D |
| #define HID_KEYBOARD_SC_F5 0x3E |
| #define HID_KEYBOARD_SC_F6 0x3F |
| #define HID_KEYBOARD_SC_F7 0x40 |
| #define HID_KEYBOARD_SC_F8 0x41 |
| #define HID_KEYBOARD_SC_F9 0x42 |
| #define HID_KEYBOARD_SC_FIND 0x7E |
| #define HID_KEYBOARD_SC_G 0x0A |
| #define HID_KEYBOARD_SC_GRAVE_ACCENT_AND_TILDE 0x35 |
| #define HID_KEYBOARD_SC_H 0x0B |
| #define HID_KEYBOARD_SC_HELP 0x75 |
| #define HID_KEYBOARD_SC_HOME 0x4A |
| #define HID_KEYBOARD_SC_I 0x0C |
| #define HID_KEYBOARD_SC_INSERT 0x49 |
| #define HID_KEYBOARD_SC_INTERNATIONAL1 0x87 |
| #define HID_KEYBOARD_SC_INTERNATIONAL2 0x88 |
| #define HID_KEYBOARD_SC_INTERNATIONAL3 0x89 |
| #define HID_KEYBOARD_SC_INTERNATIONAL4 0x8A |
| #define HID_KEYBOARD_SC_INTERNATIONAL5 0x8B |
| #define HID_KEYBOARD_SC_INTERNATIONAL6 0x8C |
| #define HID_KEYBOARD_SC_INTERNATIONAL7 0x8D |
| #define HID_KEYBOARD_SC_INTERNATIONAL8 0x8E |
| #define HID_KEYBOARD_SC_INTERNATIONAL9 0x8F |
| #define HID_KEYBOARD_SC_J 0x0D |
| #define HID_KEYBOARD_SC_K 0x0E |
| #define HID_KEYBOARD_SC_KEYPAD_00 0xB0 |
| #define HID_KEYBOARD_SC_KEYPAD_000 0xB1 |
| #define HID_KEYBOARD_SC_KEYPAD_0_AND_INSERT 0x62 |
| #define HID_KEYBOARD_SC_KEYPAD_1_AND_END 0x59 |
| #define HID_KEYBOARD_SC_KEYPAD_2_AND_DOWN_ARROW 0x5A |
| #define HID_KEYBOARD_SC_KEYPAD_3_AND_PAGE_DOWN 0x5B |
| #define HID_KEYBOARD_SC_KEYPAD_4_AND_LEFT_ARROW 0x5C |
| #define HID_KEYBOARD_SC_KEYPAD_5 0x5D |
| #define HID_KEYBOARD_SC_KEYPAD_6_AND_RIGHT_ARROW 0x5E |
| #define HID_KEYBOARD_SC_KEYPAD_7_AND_HOME 0x5F |
| #define HID_KEYBOARD_SC_KEYPAD_8_AND_UP_ARROW 0x60 |
| #define HID_KEYBOARD_SC_KEYPAD_9_AND_PAGE_UP 0x61 |
| #define HID_KEYBOARD_SC_KEYPAD_A 0xBC |
| #define HID_KEYBOARD_SC_KEYPAD_AMP 0xC7 |
| #define HID_KEYBOARD_SC_KEYPAD_AMP_AMP 0xC8 |
| #define HID_KEYBOARD_SC_KEYPAD_ASTERISK 0x55 |
| #define HID_KEYBOARD_SC_KEYPAD_AT 0xCE |
| #define HID_KEYBOARD_SC_KEYPAD_B 0xBD |
| #define HID_KEYBOARD_SC_KEYPAD_BACKSPACE 0xBB |
| #define HID_KEYBOARD_SC_KEYPAD_BINARY 0xDA |
| #define HID_KEYBOARD_SC_KEYPAD_C 0xBE |
| #define HID_KEYBOARD_SC_KEYPAD_CARET 0xC3 |
| #define HID_KEYBOARD_SC_KEYPAD_CLEAR 0xD8 |
| #define HID_KEYBOARD_SC_KEYPAD_CLEAR_ENTRY 0xD9 |
| #define HID_KEYBOARD_SC_KEYPAD_CLOSING_BRACE 0xB9 |
| #define HID_KEYBOARD_SC_KEYPAD_CLOSING_PARENTHESIS 0xB7 |
| #define HID_KEYBOARD_SC_KEYPAD_COLON 0xCB |
| #define HID_KEYBOARD_SC_KEYPAD_COMMA 0x85 |
| #define HID_KEYBOARD_SC_KEYPAD_D 0xBF |
| #define HID_KEYBOARD_SC_KEYPAD_DECIMAL 0xDC |
| #define HID_KEYBOARD_SC_KEYPAD_DOT_AND_DELETE 0x63 |
| #define HID_KEYBOARD_SC_KEYPAD_E 0xC0 |
| #define HID_KEYBOARD_SC_KEYPAD_ENTER 0x58 |
| #define HID_KEYBOARD_SC_KEYPAD_EQUAL_SIGN 0x67 |
| #define HID_KEYBOARD_SC_KEYPAD_EQUAL_SIGN_AS400 0x86 |
| #define HID_KEYBOARD_SC_KEYPAD_EXCLAMATION_SIGN 0xCF |
| #define HID_KEYBOARD_SC_KEYPAD_F 0xC1 |
| #define HID_KEYBOARD_SC_KEYPAD_GREATER_THAN_SIGN 0xC6 |
| #define HID_KEYBOARD_SC_KEYPAD_HASHMARK 0xCC |
| #define HID_KEYBOARD_SC_KEYPAD_HEXADECIMAL 0xDD |
| #define HID_KEYBOARD_SC_KEYPAD_LESS_THAN_SIGN 0xC5 |
| #define HID_KEYBOARD_SC_KEYPAD_MEMORY_ADD 0xD3 |
| #define HID_KEYBOARD_SC_KEYPAD_MEMORY_CLEAR 0xD2 |
| #define HID_KEYBOARD_SC_KEYPAD_MEMORY_DIVIDE 0xD6 |
| #define HID_KEYBOARD_SC_KEYPAD_MEMORY_MULTIPLY 0xD5 |
| #define HID_KEYBOARD_SC_KEYPAD_MEMORY_RECALL 0xD1 |
| #define HID_KEYBOARD_SC_KEYPAD_MEMORY_STORE 0xD0 |
| #define HID_KEYBOARD_SC_KEYPAD_MEMORY_SUBTRACT 0xD4 |
| #define HID_KEYBOARD_SC_KEYPAD_MINUS 0x56 |
| #define HID_KEYBOARD_SC_KEYPAD_OCTAL 0xDB |
| #define HID_KEYBOARD_SC_KEYPAD_OPENING_BRACE 0xB8 |
| #define HID_KEYBOARD_SC_KEYPAD_OPENING_PARENTHESIS 0xB6 |
| #define HID_KEYBOARD_SC_KEYPAD_PERCENTAGE 0xC4 |
| #define HID_KEYBOARD_SC_KEYPAD_PIPE 0xC9 |
| #define HID_KEYBOARD_SC_KEYPAD_PIPE_PIPE 0xCA |
| #define HID_KEYBOARD_SC_KEYPAD_PLUS 0x57 |
| #define HID_KEYBOARD_SC_KEYPAD_PLUS_AND_MINUS 0xD7 |
| #define HID_KEYBOARD_SC_KEYPAD_SLASH 0x54 |
| #define HID_KEYBOARD_SC_KEYPAD_SPACE 0xCD |
| #define HID_KEYBOARD_SC_KEYPAD_TAB 0xBA |
| #define HID_KEYBOARD_SC_KEYPAD_XOR 0xC2 |
| #define HID_KEYBOARD_SC_L 0x0F |
| #define HID_KEYBOARD_SC_LANG1 0x90 |
| #define HID_KEYBOARD_SC_LANG2 0x91 |
| #define HID_KEYBOARD_SC_LANG3 0x92 |
| #define HID_KEYBOARD_SC_LANG4 0x93 |
| #define HID_KEYBOARD_SC_LANG5 0x94 |
| #define HID_KEYBOARD_SC_LANG6 0x95 |
| #define HID_KEYBOARD_SC_LANG7 0x96 |
| #define HID_KEYBOARD_SC_LANG8 0x97 |
| #define HID_KEYBOARD_SC_LANG9 0x98 |
| #define HID_KEYBOARD_SC_LEFT_ALT 0xE2 |
| #define HID_KEYBOARD_SC_LEFT_ARROW 0x50 |
| #define HID_KEYBOARD_SC_LEFT_CONTROL 0xE0 |
| #define HID_KEYBOARD_SC_LEFT_GUI 0xE3 |
| #define HID_KEYBOARD_SC_LEFT_SHIFT 0xE1 |
| #define HID_KEYBOARD_SC_LOCKING_CAPS_LOCK 0x82 |
| #define HID_KEYBOARD_SC_LOCKING_NUM_LOCK 0x83 |
| #define HID_KEYBOARD_SC_LOCKING_SCROLL_LOCK 0x84 |
| #define HID_KEYBOARD_SC_M 0x10 |
| #define HID_KEYBOARD_SC_MANU 0x76 |
| #define HID_KEYBOARD_SC_MINUS_AND_UNDERSCORE 0x2D |
| #define HID_KEYBOARD_SC_MUTE 0x7F |
| #define HID_KEYBOARD_SC_N 0x11 |
| #define HID_KEYBOARD_SC_NON_US_BACKSLASH_AND_PIPE 0x64 |
| #define HID_KEYBOARD_SC_NON_US_HASHMARK_AND_TILDE 0x32 |
| #define HID_KEYBOARD_SC_NUM_LOCK 0x53 |
| #define HID_KEYBOARD_SC_O 0x12 |
| #define HID_KEYBOARD_SC_OPENING_BRACKET_AND_OPENING_BRACE 0x2F |
| #define HID_KEYBOARD_SC_OPER 0xA1 |
| #define HID_KEYBOARD_SC_OUT 0xA0 |
| #define HID_KEYBOARD_SC_P 0x13 |
| #define HID_KEYBOARD_SC_PAGE_DOWN 0x4E |
| #define HID_KEYBOARD_SC_PAGE_UP 0x4B |
| #define HID_KEYBOARD_SC_PASTE 0x7D |
| #define HID_KEYBOARD_SC_PAUSE 0x48 |
| #define HID_KEYBOARD_SC_POST_FAIL 0x02 |
| #define HID_KEYBOARD_SC_POWER 0x66 |
| #define HID_KEYBOARD_SC_PRINT_SCREEN 0x46 |
| #define HID_KEYBOARD_SC_PRIOR 0x9D |
| #define HID_KEYBOARD_SC_Q 0x14 |
| #define HID_KEYBOARD_SC_R 0x15 |
| #define HID_KEYBOARD_SC_RETURN 0x9E |
| #define HID_KEYBOARD_SC_RIGHT_ALT 0xE6 |
| #define HID_KEYBOARD_SC_RIGHT_ARROW 0x4F |
| #define HID_KEYBOARD_SC_RIGHT_CONTROL 0xE4 |
| #define HID_KEYBOARD_SC_RIGHT_GUI 0xE7 |
| #define HID_KEYBOARD_SC_RIGHT_SHIFT 0xE5 |
| #define HID_KEYBOARD_SC_S 0x16 |
| #define HID_KEYBOARD_SC_SCROLL_LOCK 0x47 |
| #define HID_KEYBOARD_SC_SELECT 0x77 |
| #define HID_KEYBOARD_SC_SEMICOLON_AND_COLON 0x33 |
| #define HID_KEYBOARD_SC_SEPARATOR 0x9F |
| #define HID_KEYBOARD_SC_SISREQ 0x9A |
| #define HID_KEYBOARD_SC_SLASH_AND_QUESTION_MARK 0x38 |
| #define HID_KEYBOARD_SC_SPACE 0x2C |
| #define HID_KEYBOARD_SC_STOP 0x78 |
| #define HID_KEYBOARD_SC_T 0x17 |
| #define HID_KEYBOARD_SC_TAB 0x2B |
| #define HID_KEYBOARD_SC_THOUSANDS_SEPARATOR 0xB2 |
| #define HID_KEYBOARD_SC_U 0x18 |
| #define HID_KEYBOARD_SC_UNDO 0x7A |
| #define HID_KEYBOARD_SC_UP_ARROW 0x52 |
| #define HID_KEYBOARD_SC_V 0x19 |
| #define HID_KEYBOARD_SC_VOLUME_DOWN 0x81 |
| #define HID_KEYBOARD_SC_VOLUME_UP 0x80 |
| #define HID_KEYBOARD_SC_W 0x1A |
| #define HID_KEYBOARD_SC_X 0x1B |
| #define HID_KEYBOARD_SC_Y 0x1C |
| #define HID_KEYBOARD_SC_Z 0x1D |
| typedef uint8_t USB_Descriptor_HIDReport_Datatype_t |
Type define for the data type used to store HID report descriptor elements.
| enum HID_ClassRequests_t |
Enum for the HID class specific control requests that can be issued by the USB bus host.
Enum for possible Class, Subclass and Protocol values of device and interface descriptors relating to the HID device class.