Data Structures | |
| struct | MS_CommandBlockWrapper_t |
| Mass Storage Class Command Block Wrapper. More... | |
| struct | MS_CommandStatusWrapper_t |
| Mass Storage Class Command Status Wrapper. More... | |
| struct | SCSI_Inquiry_Response_t |
| Mass Storage Class SCSI Inquiry Structure. More... | |
| struct | SCSI_Request_Sense_Response_t |
| Mass Storage Class SCSI Sense Structure. More... | |
Macros | |
| #define | MS_CBW_SIGNATURE 0x43425355UL |
| #define | MS_COMMAND_DIR_DATA_IN (1 << 7) |
| #define | MS_COMMAND_DIR_DATA_OUT (0 << 7) |
| #define | MS_CSW_SIGNATURE 0x53425355UL |
Enumerations | |
| enum | MS_ClassRequests_t { MS_REQ_GetMaxLUN = 0xFE, MS_REQ_MassStorageReset = 0xFF } |
| enum | MS_CommandStatusCodes_t { MS_SCSI_COMMAND_Pass = 0, MS_SCSI_COMMAND_Fail = 1, MS_SCSI_COMMAND_PhaseError = 2 } |
| enum | MS_Descriptor_ClassSubclassProtocol_t { MS_CSCP_MassStorageClass = 0x08, MS_CSCP_SCSITransparentSubclass = 0x06, MS_CSCP_BulkOnlyTransportProtocol = 0x50 } |
SCSI Commands | |
| #define | SCSI_CMD_INQUIRY 0x12 |
| #define | SCSI_CMD_REQUEST_SENSE 0x03 |
| #define | SCSI_CMD_TEST_UNIT_READY 0x00 |
| #define | SCSI_CMD_READ_CAPACITY_10 0x25 |
| #define | SCSI_CMD_START_STOP_UNIT 0x1B |
| #define | SCSI_CMD_SEND_DIAGNOSTIC 0x1D |
| #define | SCSI_CMD_PREVENT_ALLOW_MEDIUM_REMOVAL 0x1E |
| #define | SCSI_CMD_WRITE_10 0x2A |
| #define | SCSI_CMD_READ_10 0x28 |
| #define | SCSI_CMD_WRITE_6 0x0A |
| #define | SCSI_CMD_READ_6 0x08 |
| #define | SCSI_CMD_VERIFY_10 0x2F |
| #define | SCSI_CMD_MODE_SENSE_6 0x1A |
| #define | SCSI_CMD_MODE_SENSE_10 0x5A |
SCSI Sense Key Values | |
| #define | SCSI_SENSE_KEY_GOOD 0x00 |
| #define | SCSI_SENSE_KEY_RECOVERED_ERROR 0x01 |
| #define | SCSI_SENSE_KEY_NOT_READY 0x02 |
| #define | SCSI_SENSE_KEY_MEDIUM_ERROR 0x03 |
| #define | SCSI_SENSE_KEY_HARDWARE_ERROR 0x04 |
| #define | SCSI_SENSE_KEY_ILLEGAL_REQUEST 0x05 |
| #define | SCSI_SENSE_KEY_UNIT_ATTENTION 0x06 |
| #define | SCSI_SENSE_KEY_DATA_PROTECT 0x07 |
| #define | SCSI_SENSE_KEY_BLANK_CHECK 0x08 |
| #define | SCSI_SENSE_KEY_VENDOR_SPECIFIC 0x09 |
| #define | SCSI_SENSE_KEY_COPY_ABORTED 0x0A |
| #define | SCSI_SENSE_KEY_ABORTED_COMMAND 0x0B |
| #define | SCSI_SENSE_KEY_VOLUME_OVERFLOW 0x0D |
| #define | SCSI_SENSE_KEY_MISCOMPARE 0x0E |
SCSI Additional Sense Codes | |
| #define | SCSI_ASENSE_NO_ADDITIONAL_INFORMATION 0x00 |
| #define | SCSI_ASENSE_LOGICAL_UNIT_NOT_READY 0x04 |
| #define | SCSI_ASENSE_INVALID_FIELD_IN_CDB 0x24 |
| #define | SCSI_ASENSE_NOT_READY_TO_READY_CHANGE 0x28 |
| #define | SCSI_ASENSE_WRITE_PROTECTED 0x27 |
| #define | SCSI_ASENSE_FORMAT_ERROR 0x31 |
| #define | SCSI_ASENSE_INVALID_COMMAND 0x20 |
| #define | SCSI_ASENSE_LOGICAL_BLOCK_ADDRESS_OUT_OF_RANGE 0x21 |
| #define | SCSI_ASENSE_MEDIUM_NOT_PRESENT 0x3A |
SCSI Additional Sense Key Code Qualifiers | |
| #define | SCSI_ASENSEQ_NO_QUALIFIER 0x00 |
| #define | SCSI_ASENSEQ_FORMAT_COMMAND_FAILED 0x01 |
| #define | SCSI_ASENSEQ_INITIALIZING_COMMAND_REQUIRED 0x02 |
| #define | SCSI_ASENSEQ_OPERATION_IN_PROGRESS 0x07 |
Constants, Types and Enum definitions that are common to both Device and Host modes for the USB Mass Storage Class.
| #define MS_CBW_SIGNATURE 0x43425355UL |
Magic signature for a Command Block Wrapper used in the Mass Storage Bulk-Only transport protocol.
| #define MS_COMMAND_DIR_DATA_IN (1 << 7) |
Mask for a Command Block Wrapper's flags attribute to specify a command with data sent from device-to-host.
| #define MS_COMMAND_DIR_DATA_OUT (0 << 7) |
Mask for a Command Block Wrapper's flags attribute to specify a command with data sent from host-to-device.
| #define MS_CSW_SIGNATURE 0x53425355UL |
Magic signature for a Command Status Wrapper used in the Mass Storage Bulk-Only transport protocol.
| #define SCSI_ASENSE_FORMAT_ERROR 0x31 |
SCSI Additional Sense Code to indicate an error whilst formatting the device medium.
| #define SCSI_ASENSE_INVALID_COMMAND 0x20 |
SCSI Additional Sense Code to indicate an invalid command was issued.
| #define SCSI_ASENSE_INVALID_FIELD_IN_CDB 0x24 |
SCSI Additional Sense Code to indicate an invalid field was encountered while processing the issued command.
| #define SCSI_ASENSE_LOGICAL_BLOCK_ADDRESS_OUT_OF_RANGE 0x21 |
SCSI Additional Sense Code to indicate a write to a block out outside of the medium's range was issued.
| #define SCSI_ASENSE_LOGICAL_UNIT_NOT_READY 0x04 |
SCSI Additional Sense Code to indicate that the logical unit (LUN) addressed is not ready.
| #define SCSI_ASENSE_MEDIUM_NOT_PRESENT 0x3A |
SCSI Additional Sense Code to indicate that no removable medium is inserted into the device.
| #define SCSI_ASENSE_NO_ADDITIONAL_INFORMATION 0x00 |
SCSI Additional Sense Code to indicate no additional sense information is available.
| #define SCSI_ASENSE_NOT_READY_TO_READY_CHANGE 0x28 |
SCSI Additional Sense Code to indicate that a medium that was previously indicated as not ready has now become ready for use.
| #define SCSI_ASENSE_WRITE_PROTECTED 0x27 |
SCSI Additional Sense Code to indicate that an attempt to write to a protected area was made.
| #define SCSI_ASENSEQ_FORMAT_COMMAND_FAILED 0x01 |
SCSI Additional Sense Qualifier Code to indicate that a medium format command failed to complete.
| #define SCSI_ASENSEQ_INITIALIZING_COMMAND_REQUIRED 0x02 |
SCSI Additional Sense Qualifier Code to indicate that an initializing command must be issued before the issued command can be executed.
| #define SCSI_ASENSEQ_NO_QUALIFIER 0x00 |
SCSI Additional Sense Qualifier Code to indicate no additional sense qualifier information is available.
| #define SCSI_ASENSEQ_OPERATION_IN_PROGRESS 0x07 |
SCSI Additional Sense Qualifier Code to indicate that an operation is currently in progress.
| #define SCSI_CMD_INQUIRY 0x12 |
SCSI Command Code for an INQUIRY command.
| #define SCSI_CMD_MODE_SENSE_10 0x5A |
SCSI Command Code for a MODE SENSE (10) command.
| #define SCSI_CMD_MODE_SENSE_6 0x1A |
SCSI Command Code for a MODE SENSE (6) command.
| #define SCSI_CMD_PREVENT_ALLOW_MEDIUM_REMOVAL 0x1E |
SCSI Command Code for a PREVENT ALLOW MEDIUM REMOVAL command.
| #define SCSI_CMD_READ_10 0x28 |
SCSI Command Code for a READ (10) command.
| #define SCSI_CMD_READ_6 0x08 |
SCSI Command Code for a READ (6) command.
| #define SCSI_CMD_READ_CAPACITY_10 0x25 |
SCSI Command Code for a READ CAPACITY (10) command.
| #define SCSI_CMD_REQUEST_SENSE 0x03 |
SCSI Command Code for a REQUEST SENSE command.
| #define SCSI_CMD_SEND_DIAGNOSTIC 0x1D |
SCSI Command Code for a SEND DIAGNOSTIC command.
| #define SCSI_CMD_START_STOP_UNIT 0x1B |
SCSI Command Code for a START STOP UNIT command.
| #define SCSI_CMD_TEST_UNIT_READY 0x00 |
SCSI Command Code for a TEST UNIT READY command.
| #define SCSI_CMD_VERIFY_10 0x2F |
SCSI Command Code for a VERIFY (10) command.
| #define SCSI_CMD_WRITE_10 0x2A |
SCSI Command Code for a WRITE (10) command.
| #define SCSI_CMD_WRITE_6 0x0A |
SCSI Command Code for a WRITE (6) command.
| #define SCSI_SENSE_KEY_ABORTED_COMMAND 0x0B |
SCSI Sense Code to indicate that the device has aborted the issued command.
| #define SCSI_SENSE_KEY_BLANK_CHECK 0x08 |
SCSI Sense Code to indicate an error while trying to write to a write-once medium.
| #define SCSI_SENSE_KEY_COPY_ABORTED 0x0A |
SCSI Sense Code to indicate that an EXTENDED COPY command has aborted due to an error.
| #define SCSI_SENSE_KEY_DATA_PROTECT 0x07 |
SCSI Sense Code to indicate that a write attempt on a protected block has been made.
| #define SCSI_SENSE_KEY_GOOD 0x00 |
SCSI Sense Code to indicate no error has occurred.
| #define SCSI_SENSE_KEY_HARDWARE_ERROR 0x04 |
SCSI Sense Code to indicate a hardware error has occurred.
| #define SCSI_SENSE_KEY_ILLEGAL_REQUEST 0x05 |
SCSI Sense Code to indicate that an illegal request has been issued.
| #define SCSI_SENSE_KEY_MEDIUM_ERROR 0x03 |
SCSI Sense Code to indicate an error whilst accessing the medium.
| #define SCSI_SENSE_KEY_MISCOMPARE 0x0E |
SCSI Sense Code to indicate that the source data did not match the data read from the medium.
| #define SCSI_SENSE_KEY_NOT_READY 0x02 |
SCSI Sense Code to indicate that the device is not ready for a new command.
| #define SCSI_SENSE_KEY_RECOVERED_ERROR 0x01 |
SCSI Sense Code to indicate that the device has recovered from an error.
| #define SCSI_SENSE_KEY_UNIT_ATTENTION 0x06 |
SCSI Sense Code to indicate that the unit requires attention from the host to indicate a reset event, medium removal or other condition.
| #define SCSI_SENSE_KEY_VENDOR_SPECIFIC 0x09 |
SCSI Sense Code to indicate a vendor specific error has occurred.
| #define SCSI_SENSE_KEY_VOLUME_OVERFLOW 0x0D |
SCSI Sense Code to indicate an attempt to write past the end of a partition has been made.
| enum MS_ClassRequests_t |
Enum for the Mass Storage class specific control requests that can be issued by the USB bus host.
Enum for the possible command status wrapper return status codes.
Enum for possible Class, Subclass and Protocol values of device and interface descriptors relating to the Mass Storage device class.