|
| uint8_t | MS_Host_ConfigurePipes (USB_ClassInfo_MS_Host_t *const MSInterfaceInfo, uint16_t ConfigDescriptorSize, void *DeviceConfigDescriptor) ATTR_NON_NULL_PTR_ARG(1) ATTR_NON_NULL_PTR_ARG(3) |
| |
| uint8_t | MS_Host_GetInquiryData (USB_ClassInfo_MS_Host_t *const MSInterfaceInfo, const uint8_t LUNIndex, SCSI_Inquiry_Response_t *const InquiryData) ATTR_NON_NULL_PTR_ARG(1) ATTR_NON_NULL_PTR_ARG(3) |
| |
| uint8_t | MS_Host_GetMaxLUN (USB_ClassInfo_MS_Host_t *const MSInterfaceInfo, uint8_t *const MaxLUNIndex) ATTR_NON_NULL_PTR_ARG(1) ATTR_NON_NULL_PTR_ARG(2) |
| |
| uint8_t | MS_Host_PreventAllowMediumRemoval (USB_ClassInfo_MS_Host_t *const MSInterfaceInfo, const uint8_t LUNIndex, const bool PreventRemoval) ATTR_NON_NULL_PTR_ARG(1) |
| |
| uint8_t | MS_Host_ReadDeviceBlocks (USB_ClassInfo_MS_Host_t *const MSInterfaceInfo, const uint8_t LUNIndex, const uint32_t BlockAddress, const uint8_t Blocks, const uint16_t BlockSize, void *BlockBuffer) ATTR_NON_NULL_PTR_ARG(1) ATTR_NON_NULL_PTR_ARG(6) |
| |
| uint8_t | MS_Host_ReadDeviceCapacity (USB_ClassInfo_MS_Host_t *const MSInterfaceInfo, const uint8_t LUNIndex, SCSI_Capacity_t *const DeviceCapacity) ATTR_NON_NULL_PTR_ARG(1) ATTR_NON_NULL_PTR_ARG(3) |
| |
| uint8_t | MS_Host_RequestSense (USB_ClassInfo_MS_Host_t *const MSInterfaceInfo, const uint8_t LUNIndex, SCSI_Request_Sense_Response_t *const SenseData) ATTR_NON_NULL_PTR_ARG(1) ATTR_NON_NULL_PTR_ARG(3) |
| |
| uint8_t | MS_Host_ResetMSInterface (USB_ClassInfo_MS_Host_t *const MSInterfaceInfo) ATTR_NON_NULL_PTR_ARG(1) |
| |
| uint8_t | MS_Host_TestUnitReady (USB_ClassInfo_MS_Host_t *const MSInterfaceInfo, const uint8_t LUNIndex) ATTR_NON_NULL_PTR_ARG(1) |
| |
| static void | MS_Host_USBTask (USB_ClassInfo_MS_Host_t *const MSInterfaceInfo) ATTR_NON_NULL_PTR_ARG(1) ATTR_ALWAYS_INLINE |
| |
| uint8_t | MS_Host_WriteDeviceBlocks (USB_ClassInfo_MS_Host_t *const MSInterfaceInfo, const uint8_t LUNIndex, const uint32_t BlockAddress, const uint8_t Blocks, const uint16_t BlockSize, const void *BlockBuffer) ATTR_NON_NULL_PTR_ARG(1) ATTR_NON_NULL_PTR_ARG(6) |
| |
Module Source Dependencies
The following files must be built with any user project that uses this module:
- LUFA/Drivers/USB/Class/Host/MassStorageClassHost.c (Makefile source module name: LUFA_SRC_USBCLASS)
Module Description
Host Mode USB Class driver framework interface, for the Mass Storage USB Class driver.
| #define MS_ERROR_LOGICAL_CMD_FAILED 0x80 |
Error code for some Mass Storage Host functions, indicating a logical (and not hardware) error.
Enum for the possible error codes returned by the MS_Host_ConfigurePipes() function.
| Enumerator |
|---|
| MS_ENUMERROR_NoError |
Configuration Descriptor was processed successfully.
|
| MS_ENUMERROR_InvalidConfigDescriptor |
The device returned an invalid Configuration Descriptor.
|
| MS_ENUMERROR_NoCompatibleInterfaceFound |
A compatible Mass Storage interface was not found in the device's Configuration Descriptor.
|
| MS_ENUMERROR_PipeConfigurationFailed |
One or more pipes for the specified interface could not be configured correctly.
|
| uint8_t MS_Host_ConfigurePipes |
( |
USB_ClassInfo_MS_Host_t *const |
MSInterfaceInfo, |
|
|
uint16_t |
ConfigDescriptorSize, |
|
|
void * |
DeviceConfigDescriptor |
|
) |
| |
Host interface configuration routine, to configure a given Mass Storage host interface instance using the Configuration Descriptor read from an attached USB device. This function automatically updates the given Mass Storage Host instance's state values and configures the pipes required to communicate with the interface if it is found within the device. This should be called once after the stack has enumerated the attached device, while the host state machine is in the Addressed state.
- Parameters
-
| [in,out] | MSInterfaceInfo | Pointer to a structure containing an MS Class host configuration and state. |
| [in] | ConfigDescriptorSize | Length of the attached device's Configuration Descriptor. |
| [in] | DeviceConfigDescriptor | Pointer to a buffer containing the attached device's Configuration Descriptor. |
- Returns
- A value from the MS_Host_EnumerationFailure_ErrorCodes_t enum.
Retrieves the Mass Storage device's inquiry data for the specified LUN, indicating the device characteristics and properties.
- Precondition
- This function must only be called when the Host state machine is in the HOST_STATE_Configured state or the call will fail.
- Parameters
-
| [in,out] | MSInterfaceInfo | Pointer to a structure containing a MS Class host configuration and state. |
| [in] | LUNIndex | LUN index within the device the command is being issued to. |
| [out] | InquiryData | Location where the read inquiry data should be stored. |
- Returns
- A value from the Pipe_Stream_RW_ErrorCodes_t enum or MS_ERROR_LOGICAL_CMD_FAILED.
Sends a GET MAX LUN control request to the attached device, retrieving the index of the highest LUN (Logical UNit, a logical drive) in the device. This value can then be used in the other functions of the Mass Storage Host mode Class driver to address a specific LUN within the device.
- Note
- Some devices do not support this request, and will STALL it when issued. To get around this, on unsupported devices the max LUN index will be reported as zero and no error will be returned if the device STALLs the request.
- Parameters
-
| [in,out] | MSInterfaceInfo | Pointer to a structure containing a MS Class host configuration and state. |
| [out] | MaxLUNIndex | Pointer to a location where the highest LUN index value should be stored. |
- Returns
- A value from the USB_Host_SendControlErrorCodes_t enum.
| uint8_t MS_Host_PreventAllowMediumRemoval |
( |
USB_ClassInfo_MS_Host_t *const |
MSInterfaceInfo, |
|
|
const uint8_t |
LUNIndex, |
|
|
const bool |
PreventRemoval |
|
) |
| |
Issues a PREVENT MEDIUM REMOVAL command, to logically (or, depending on the type of device, physically) lock the device from removal so that blocks of data on the medium can be read or altered.
- Precondition
- This function must only be called when the Host state machine is in the HOST_STATE_Configured state or the call will fail.
- Parameters
-
| [in,out] | MSInterfaceInfo | Pointer to a structure containing a MS Class host configuration and state. |
| [in] | LUNIndex | LUN index within the device the command is being issued to. |
| [in] | PreventRemoval | Boolean true if the device should be locked from removal, false otherwise. |
- Returns
- A value from the Pipe_Stream_RW_ErrorCodes_t enum or MS_ERROR_LOGICAL_CMD_FAILED if not ready.
| uint8_t MS_Host_ReadDeviceBlocks |
( |
USB_ClassInfo_MS_Host_t *const |
MSInterfaceInfo, |
|
|
const uint8_t |
LUNIndex, |
|
|
const uint32_t |
BlockAddress, |
|
|
const uint8_t |
Blocks, |
|
|
const uint16_t |
BlockSize, |
|
|
void * |
BlockBuffer |
|
) |
| |
Reads blocks of data from the attached Mass Storage device's medium.
- Precondition
- This function must only be called when the Host state machine is in the HOST_STATE_Configured state or the call will fail.
- Parameters
-
| [in,out] | MSInterfaceInfo | Pointer to a structure containing a MS Class host configuration and state. |
| [in] | LUNIndex | LUN index within the device the command is being issued to. |
| [in] | BlockAddress | Starting block address within the device to read from. |
| [in] | Blocks | Total number of blocks to read. |
| [in] | BlockSize | Size in bytes of each block within the device. |
| [out] | BlockBuffer | Pointer to where the read data from the device should be stored. |
- Returns
- A value from the Pipe_Stream_RW_ErrorCodes_t enum or MS_ERROR_LOGICAL_CMD_FAILED if not ready.
Retrieves the total capacity of the attached USB Mass Storage device, in blocks, and block size.
- Precondition
- This function must only be called when the Host state machine is in the HOST_STATE_Configured state or the call will fail.
- Parameters
-
| [in,out] | MSInterfaceInfo | Pointer to a structure containing a MS Class host configuration and state. |
| [in] | LUNIndex | LUN index within the device the command is being issued to. |
| [out] | DeviceCapacity | Pointer to the location where the capacity information should be stored. |
- Returns
- A value from the Pipe_Stream_RW_ErrorCodes_t enum or MS_ERROR_LOGICAL_CMD_FAILED if not ready.
Retrieves the device sense data, indicating the current device state and error codes for the previously issued command.
- Precondition
- This function must only be called when the Host state machine is in the HOST_STATE_Configured state or the call will fail.
- Parameters
-
| [in,out] | MSInterfaceInfo | Pointer to a structure containing a MS Class host configuration and state. |
| [in] | LUNIndex | LUN index within the device the command is being issued to. |
| [out] | SenseData | Pointer to the location where the sense information should be stored. |
- Returns
- A value from the Pipe_Stream_RW_ErrorCodes_t enum or MS_ERROR_LOGICAL_CMD_FAILED if not ready.
Sends a MASS STORAGE RESET control request to the attached device, resetting the Mass Storage Interface and readying it for the next Mass Storage command. This should be called after a failed SCSI request to ensure the attached Mass Storage device is ready to receive the next command.
- Parameters
-
| [in,out] | MSInterfaceInfo | Pointer to a structure containing a MS Class host configuration and state. |
- Returns
- A value from the USB_Host_SendControlErrorCodes_t enum.
Sends a TEST UNIT READY command to the device, to determine if it is ready to accept other SCSI commands.
- Parameters
-
| [in,out] | MSInterfaceInfo | Pointer to a structure containing a MS Class host configuration and state. |
| [in] | LUNIndex | LUN index within the device the command is being issued to. |
- Returns
- A value from the Pipe_Stream_RW_ErrorCodes_t enum or MS_ERROR_LOGICAL_CMD_FAILED if not ready.
General management task for a given Mass Storage host class interface, required for the correct operation of the interface. This should be called frequently in the main program loop, before the master USB management task USB_USBTask().
- Parameters
-
| [in,out] | MSInterfaceInfo | Pointer to a structure containing an Mass Storage Class host configuration and state. |
| uint8_t MS_Host_WriteDeviceBlocks |
( |
USB_ClassInfo_MS_Host_t *const |
MSInterfaceInfo, |
|
|
const uint8_t |
LUNIndex, |
|
|
const uint32_t |
BlockAddress, |
|
|
const uint8_t |
Blocks, |
|
|
const uint16_t |
BlockSize, |
|
|
const void * |
BlockBuffer |
|
) |
| |
Writes blocks of data to the attached Mass Storage device's medium.
- Precondition
- This function must only be called when the Host state machine is in the HOST_STATE_Configured state or the call will fail.
- Parameters
-
| [in,out] | MSInterfaceInfo | Pointer to a structure containing a MS Class host configuration and state. |
| [in] | LUNIndex | LUN index within the device the command is being issued to. |
| [in] | BlockAddress | Starting block address within the device to write to. |
| [in] | Blocks | Total number of blocks to read. |
| [in] | BlockSize | Size in bytes of each block within the device. |
| [in] | BlockBuffer | Pointer to where the data to write should be sourced from. |
- Returns
- A value from the Pipe_Stream_RW_ErrorCodes_t enum or MS_ERROR_LOGICAL_CMD_FAILED if not ready.