USB class driver for the Microsoft Remote Network Driver Interface Specification (RNDIS) class standard. More...
Modules | |
| Common Class Definitions | |
| RNDIS Class Device Mode Driver | |
| RNDIS Class Host Mode Driver | |
The following files must be built with any user project that uses this module:
RNDIS Class Driver module. This module contains an internal implementation of the Microsoft USB RNDIS Networking Class, for both Device and Host USB modes. User applications can use this class driver instead of implementing the RNDIS class manually via the low-level LUFA APIs.
This module is designed to simplify the user code by exposing only the required interface needed to interface with Hosts using the USB RNDIS Class.