Module Description
Constants, Types and Enum definitions that are common to both Device and Host modes for the USB RNDIS Class.
| #define ETHERNET_FRAME_SIZE_MAX 1500 |
Maximum size in bytes of an Ethernet frame according to the Ethernet standard.
| #define OID_802_3_CURRENT_ADDRESS 0x01010102UL |
| #define OID_802_3_MAXIMUM_LIST_SIZE 0x01010104UL |
| #define OID_802_3_MULTICAST_LIST 0x01010103UL |
| #define OID_802_3_PERMANENT_ADDRESS 0x01010101UL |
| #define OID_802_3_RCV_ERROR_ALIGNMENT 0x01020101UL |
| #define OID_802_3_XMIT_MORE_COLLISIONS 0x01020103UL |
| #define OID_802_3_XMIT_ONE_COLLISION 0x01020102UL |
| #define OID_GEN_CURRENT_PACKET_FILTER 0x0001010EUL |
| #define OID_GEN_HARDWARE_STATUS 0x00010102UL |
| #define OID_GEN_LINK_SPEED 0x00010107UL |
| #define OID_GEN_MAXIMUM_FRAME_SIZE 0x00010106UL |
| #define OID_GEN_MAXIMUM_TOTAL_SIZE 0x00010111UL |
| #define OID_GEN_MAXIMUM_TOTAL_SIZE 0x00010111UL |
| #define OID_GEN_MEDIA_CONNECT_STATUS 0x00010114UL |
| #define OID_GEN_MEDIA_IN_USE 0x00010104UL |
| #define OID_GEN_MEDIA_SUPPORTED 0x00010103UL |
| #define OID_GEN_PHYSICAL_MEDIUM 0x00010202UL |
| #define OID_GEN_RCV_ERROR 0x00020104UL |
| #define OID_GEN_RCV_NO_BUFFER 0x00020105UL |
| #define OID_GEN_RCV_OK 0x00020102UL |
| #define OID_GEN_RECEIVE_BLOCK_SIZE 0x0001010BUL |
| #define OID_GEN_SUPPORTED_LIST 0x00010101UL |
| #define OID_GEN_TRANSMIT_BLOCK_SIZE 0x0001010AUL |
| #define OID_GEN_VENDOR_DESCRIPTION 0x0001010DUL |
| #define OID_GEN_VENDOR_ID 0x0001010CUL |
| #define OID_GEN_XMIT_ERROR 0x00020103UL |
| #define OID_GEN_XMIT_OK 0x00020101UL |
| #define REMOTE_NDIS_DF_CONNECTION_ORIENTED 0x00000002UL |
| #define REMOTE_NDIS_DF_CONNECTIONLESS 0x00000001UL |
| #define REMOTE_NDIS_HALT_MSG 0x00000003UL |
| #define REMOTE_NDIS_INDICATE_STATUS_MSG 0x00000007UL |
| #define REMOTE_NDIS_INITIALIZE_CMPLT 0x80000002UL |
| #define REMOTE_NDIS_INITIALIZE_MSG 0x00000002UL |
| #define REMOTE_NDIS_KEEPALIVE_CMPLT 0x80000008UL |
| #define REMOTE_NDIS_KEEPALIVE_MSG 0x00000008UL |
| #define REMOTE_NDIS_MEDIA_STATE_CONNECTED 0x00000000UL |
| #define REMOTE_NDIS_MEDIA_STATE_DISCONNECTED 0x00000001UL |
| #define REMOTE_NDIS_MEDIUM_802_3 0x00000000UL |
| #define REMOTE_NDIS_PACKET_ALL_FUNCTIONAL 0x00002000UL |
| #define REMOTE_NDIS_PACKET_ALL_LOCAL 0x00000080UL |
| #define REMOTE_NDIS_PACKET_ALL_MULTICAST 0x00000004UL |
| #define REMOTE_NDIS_PACKET_BROADCAST 0x00000008UL |
| #define REMOTE_NDIS_PACKET_DIRECTED 0x00000001UL |
| #define REMOTE_NDIS_PACKET_FUNCTIONAL 0x00004000UL |
| #define REMOTE_NDIS_PACKET_GROUP 0x00001000UL |
| #define REMOTE_NDIS_PACKET_MAC_FRAME 0x00008000UL |
| #define REMOTE_NDIS_PACKET_MSG 0x00000001UL |
| #define REMOTE_NDIS_PACKET_MULTICAST 0x00000002UL |
| #define REMOTE_NDIS_PACKET_PROMISCUOUS 0x00000020UL |
| #define REMOTE_NDIS_PACKET_SMT 0x00000040UL |
| #define REMOTE_NDIS_PACKET_SOURCE_ROUTING 0x00000010UL |
| #define REMOTE_NDIS_QUERY_CMPLT 0x80000004UL |
| #define REMOTE_NDIS_QUERY_MSG 0x00000004UL |
| #define REMOTE_NDIS_RESET_CMPLT 0x80000006UL |
| #define REMOTE_NDIS_RESET_MSG 0x00000006UL |
| #define REMOTE_NDIS_SET_CMPLT 0x80000005UL |
| #define REMOTE_NDIS_SET_MSG 0x00000005UL |
| #define REMOTE_NDIS_STATUS_FAILURE 0xC0000001UL |
| #define REMOTE_NDIS_STATUS_INVALID_DATA 0xC0010015UL |
| #define REMOTE_NDIS_STATUS_MEDIA_CONNECT 0x4001000BUL |
| #define REMOTE_NDIS_STATUS_MEDIA_DISCONNECT 0x4001000CUL |
| #define REMOTE_NDIS_STATUS_NOT_SUPPORTED 0xC00000BBUL |
| #define REMOTE_NDIS_STATUS_SUCCESS 0x00000000UL |
| #define REMOTE_NDIS_VERSION_MAJOR 0x01 |
Implemented RNDIS Version Major.
| #define REMOTE_NDIS_VERSION_MINOR 0x00 |
Implemented RNDIS Version Minor.
| #define RNDIS_ERROR_LOGICAL_CMD_FAILED 0x80 |
Additional error code for RNDIS functions when a device returns a logical command failure.
| #define RNDIS_MESSAGE_BUFFER_SIZE 128 |
Maximum size in bytes of a RNDIS control message which can be sent or received.
Enum for the NDIS hardware states.
| Enumerator |
|---|
| NDIS_HardwareStatus_Ready |
Hardware Ready to accept commands from the host.
|
| NDIS_HardwareStatus_Initializing |
Hardware busy initializing.
|
| NDIS_HardwareStatus_Reset |
Hardware reset.
|
| NDIS_HardwareStatus_Closing |
Hardware currently closing.
|
| NDIS_HardwareStatus_NotReady |
Hardware not ready to accept commands from the host.
|
Enum for the RNDIS class specific notification requests that can be issued by a RNDIS device to a host.
| Enumerator |
|---|
| RNDIS_NOTIF_ResponseAvailable |
Notification request value for a RNDIS Response Available notification.
|
Enum for the RNDIS class specific control requests that can be issued by the USB bus host.
| Enumerator |
|---|
| RNDIS_REQ_SendEncapsulatedCommand |
RNDIS request to issue a host-to-device NDIS command.
|
| RNDIS_REQ_GetEncapsulatedResponse |
RNDIS request to issue a device-to-host NDIS response.
|
Enum for the possible NDIS adapter states.
| Enumerator |
|---|
| RNDIS_Uninitialized |
Adapter currently uninitialized.
|
| RNDIS_Initialized |
Adapter currently initialized but not ready for data transfers.
|
| RNDIS_Data_Initialized |
Adapter currently initialized and ready for data transfers.
|