USB class driver for the USB-IF Still Image (PIMA-compliant) class standard. More...
Modules | |
| Common Class Definitions | |
| Still Image Class Host Mode Driver | |
The following files must be built with any user project that uses this module:
Still Image Class Driver module. This module contains an internal implementation of the USB Still Image Class, for USB Host mode only. User applications can use this class driver instead of implementing the Still Image class manually via the low-level LUFA APIs.
This module is designed to simplify the user code by exposing only the required interface needed to interface with Devices using the USB Still Image Class.