Data Structures | |
| struct | PIMA_Container_t |
| PIMA Still Image Device Command/Response Container. More... | |
Macros | |
| #define | PIMA_COMMAND_SIZE(Params) ((sizeof(PIMA_Container_t) - 12) + ((Params) * sizeof(uint32_t))) |
| #define | PIMA_DATA_SIZE(DataLen) ((sizeof(PIMA_Container_t) - 12) + (DataLen)) |
| #define | UNICODE_STRING_LENGTH(Chars) ((Chars) << 1) |
Enumerations | |
| enum | PIMA_Container_Types_t { PIMA_CONTAINER_Undefined = 0, PIMA_CONTAINER_CommandBlock = 1, PIMA_CONTAINER_DataBlock = 2, PIMA_CONTAINER_ResponseBlock = 3, PIMA_CONTAINER_EventBlock = 4 } |
| enum | PIMA_ResponseCodes_t { PIMA_RESPONSE_OK = 1, PIMA_RESPONSE_GeneralError = 2, PIMA_RESPONSE_SessionNotOpen = 3, PIMA_RESPONSE_InvalidTransaction = 4, PIMA_RESPONSE_OperationNotSupported = 5, PIMA_RESPONSE_ParameterNotSupported = 6 } |
| enum | SI_Descriptor_ClassSubclassProtocol_t { SI_CSCP_StillImageClass = 0x06, SI_CSCP_StillImageSubclass = 0x01, SI_CSCP_BulkOnlyProtocol = 0x01 } |
Constants, Types and Enum definitions that are common to both Device and Host modes for the USB Still Image Class.
| #define PIMA_COMMAND_SIZE | ( | Params | ) | ((sizeof(PIMA_Container_t) - 12) + ((Params) * sizeof(uint32_t))) |
Used in the DataLength field of a PIMA container, to give the total container size in bytes for a command container.
| [in] | Params | Number of parameters which are to be sent in the Param field of the container. |
| #define PIMA_DATA_SIZE | ( | DataLen | ) | ((sizeof(PIMA_Container_t) - 12) + (DataLen)) |
Used in the DataLength field of a PIMA container, to give the total container size in bytes for a data container.
| [in] | DataLen | Length in bytes of the data in the container. |
| #define UNICODE_STRING_LENGTH | ( | Chars | ) | ((Chars) << 1) |
Length in bytes of a given Unicode string's character length.
| [in] | Chars | Total number of Unicode characters in the string. |
Enum for the possible PIMA contains types.
| enum PIMA_ResponseCodes_t |
Enums for the possible status codes of a returned Response Block from an attached PIMA compliant Still Image device.
Enum for possible Class, Subclass and Protocol values of device and interface descriptors relating to the Still Image device class.