USB Controller definitions for general USB controller management. More...
Modules | |
| USB Interface Management (AVR8) | |
| USB Controller definitions for the AVR8 microcontrollers. | |
| USB Interface Management (EFM32GG) | |
| USB Controller definitions for the EFM32 Giant Gecko microcontrollers. | |
| USB Interface Management (UC3) | |
| USB Controller definitions for the AVR32 UC3 microcontrollers. | |
| USB Interface Management (XMEGA) | |
| USB Controller definitions for the AVR XMEGA microcontrollers. | |
Enumerations | |
| enum | USB_Modes_t { USB_MODE_None = 0, USB_MODE_Device = 1, USB_MODE_Host = 2, USB_MODE_UID = 3 } |
Functions | |
| void | USB_USBTask (void) |
Variables | |
| USB_Request_Header_t | USB_ControlRequest |
| volatile bool | USB_IsInitialized |
Endpoint Direction Masks | |
| #define | ENDPOINT_DIR_MASK 0x80 |
| #define | ENDPOINT_DIR_OUT 0x00 |
| #define | ENDPOINT_DIR_IN 0x80 |
Pipe Direction Masks | |
| #define | PIPE_DIR_MASK 0x80 |
| #define | PIPE_DIR_OUT 0x00 |
| #define | PIPE_DIR_IN 0x80 |
Endpoint/Pipe Type Masks | |
| #define | EP_TYPE_MASK 0x03 |
| #define | EP_TYPE_CONTROL 0x00 |
| #define | EP_TYPE_ISOCHRONOUS 0x01 |
| #define | EP_TYPE_BULK 0x02 |
| #define | EP_TYPE_INTERRUPT 0x03 |
Functions, macros, variables, enums and types related to the setup and management of the USB interface.
| #define ENDPOINT_DIR_IN 0x80 |
Endpoint address direction mask for an IN direction (Device to Host) endpoint. This may be ORed with the index of the address within a device to obtain the full endpoint address.
| #define ENDPOINT_DIR_MASK 0x80 |
Endpoint direction mask, for masking against endpoint addresses to retrieve the endpoint's direction for comparing with the ENDPOINT_DIR_* masks.
| #define ENDPOINT_DIR_OUT 0x00 |
Endpoint address direction mask for an OUT direction (Host to Device) endpoint. This may be ORed with the index of the address within a device to obtain the full endpoint address.
| #define EP_TYPE_BULK 0x02 |
Mask for a BULK type endpoint or pipe.
| #define EP_TYPE_CONTROL 0x00 |
Mask for a CONTROL type endpoint or pipe.
| #define EP_TYPE_INTERRUPT 0x03 |
Mask for an INTERRUPT type endpoint or pipe.
| #define EP_TYPE_ISOCHRONOUS 0x01 |
Mask for an ISOCHRONOUS type endpoint or pipe.
| #define EP_TYPE_MASK 0x03 |
Mask for determining the type of an endpoint from an endpoint descriptor. This should then be compared with the EP_TYPE_* masks to determine the exact type of the endpoint.
| #define PIPE_DIR_IN 0x80 |
Endpoint address direction mask for an IN direction (Device to Host) endpoint. This may be ORed with the index of the address within a device to obtain the full endpoint address.
| #define PIPE_DIR_MASK 0x80 |
Pipe direction mask, for masking against pipe addresses to retrieve the pipe's direction for comparing with the PIPE_DIR_* masks.
| #define PIPE_DIR_OUT 0x00 |
Endpoint address direction mask for an OUT direction (Host to Device) endpoint. This may be ORed with the index of the address within a device to obtain the full endpoint address.
| enum USB_Modes_t |
Enum for the possible USB controller modes, for initialization via USB_Init() and indication back to the user application via USB_CurrentMode.
| void USB_USBTask | ( | void | ) |
This is the main USB management task. The USB driver requires this task to be executed continuously when the USB system is active (device attached in host mode, or attached to a host in device mode) in order to manage USB communications. This task may be executed inside an RTOS, fast timer ISR or the main user application loop.
The USB task must be serviced within 30ms while in device mode, or within 1ms while in host mode. The task may be serviced at all times, or (for minimum CPU consumption):
If in device mode (only), the control endpoint can instead be managed via interrupts entirely by the library by defining the INTERRUPT_CONTROL_ENDPOINT token and passing it to the compiler via the -D switch.
| USB_Request_Header_t USB_ControlRequest |
Structure containing the last received Control request when in Device mode (for use in user-applications inside of the EVENT_USB_Device_ControlRequest() event, or for filling up with a control request to issue when in Host mode before calling USB_Host_SendControlRequest().
| volatile bool USB_IsInitialized |
Indicates if the USB interface is currently initialized but not necessarily connected to a host or device (i.e. if USB_Init() has been run). If this is false, all other library globals related to the USB driver are invalid.