CDC Virtual Serial Port Line Encoding Settings Structure. More...
#include <CDCClassCommon.h>
Data Fields | |
| uint32_t | BaudRateBPS |
| uint8_t | CharFormat |
| uint8_t | DataBits |
| uint8_t | ParityType |
Type define for a CDC Line Encoding structure, used to hold the various encoding parameters for a virtual serial port.
| uint32_t CDC_LineEncoding_t::BaudRateBPS |
Baud rate of the virtual serial port, in bits per second.
| uint8_t CDC_LineEncoding_t::CharFormat |
Character format of the virtual serial port, a value from the CDC_LineEncodingFormats_t enum.
| uint8_t CDC_LineEncoding_t::DataBits |
Bits of data per character of the virtual serial port.
| uint8_t CDC_LineEncoding_t::ParityType |
Parity setting of the virtual serial port, a value from the CDC_LineEncodingParity_t enum.