HID Parser State Structure. More...
#include <HIDParser.h>
Data Fields | |
| HID_CollectionPath_t | CollectionPaths [HID_MAX_COLLECTIONS] |
| uint16_t | LargestReportSizeBits |
| HID_ReportSizeInfo_t | ReportIDSizes [HID_MAX_REPORT_IDS] |
| HID_ReportItem_t | ReportItems [HID_MAX_REPORTITEMS] |
| uint8_t | TotalDeviceReports |
| uint8_t | TotalReportItems |
| bool | UsingReportIDs |
Type define for a complete processed HID report, including all report item data and collections.
| HID_CollectionPath_t HID_ReportInfo_t::CollectionPaths[HID_MAX_COLLECTIONS] |
All collection items, referenced by the report items.
| uint16_t HID_ReportInfo_t::LargestReportSizeBits |
Largest report that the attached device will generate, in bits
| HID_ReportSizeInfo_t HID_ReportInfo_t::ReportIDSizes[HID_MAX_REPORT_IDS] |
Report sizes for each report in the interface
| HID_ReportItem_t HID_ReportInfo_t::ReportItems[HID_MAX_REPORTITEMS] |
Report items array, including all IN, OUT and FEATURE items.
| uint8_t HID_ReportInfo_t::TotalDeviceReports |
Number of reports within the HID interface
| uint8_t HID_ReportInfo_t::TotalReportItems |
Total number of report items stored in the ReportItems array.
| bool HID_ReportInfo_t::UsingReportIDs |
Indicates if the device has at least one REPORT ID element in its HID report descriptor.