MIDI Class Driver Event Packet. More...
#include <MIDIClassCommon.h>
Data Fields | |
| uint8_t | Data1 |
| uint8_t | Data2 |
| uint8_t | Data3 |
| uint8_t | Event |
Type define for a USB MIDI event packet, used to encapsulate sent and received MIDI messages from a USB MIDI interface.
| uint8_t MIDI_EventPacket_t::Data1 |
First byte of data in the MIDI event.
| uint8_t MIDI_EventPacket_t::Data2 |
Second byte of data in the MIDI event.
| uint8_t MIDI_EventPacket_t::Data3 |
Third byte of data in the MIDI event.
| uint8_t MIDI_EventPacket_t::Event |
MIDI event type, constructed with the MIDI_EVENT() macro.