Mass Storage Class Command Status Wrapper. More...
#include <MassStorageClassCommon.h>
Data Fields | |
| uint32_t | DataTransferResidue |
| uint32_t | Signature |
| uint8_t | Status |
| uint32_t | Tag |
Type define for a Command Status Wrapper, used in the Mass Storage Bulk-Only Transport protocol.
| uint32_t MS_CommandStatusWrapper_t::DataTransferResidue |
Number of bytes of data not processed in the SCSI command.
| uint32_t MS_CommandStatusWrapper_t::Signature |
Status block signature, must be MS_CSW_SIGNATURE to indicate a valid Command Status.
| uint8_t MS_CommandStatusWrapper_t::Status |
Status code of the issued command - a value from the MS_CommandStatusCodes_t enum.
| uint32_t MS_CommandStatusWrapper_t::Tag |
Unique command ID value, to associate a command block wrapper with its command status wrapper.