PIMA Still Image Device Command/Response Container. More...
#include <StillImageClassCommon.h>
Data Fields | |
| uint16_t | Code |
| uint32_t | DataLength |
| uint32_t | Params [3] |
| uint32_t | TransactionID |
| uint16_t | Type |
Type define for a PIMA container, use to send commands and receive responses to and from an attached Still Image device.
| uint16_t PIMA_Container_t::Code |
Command, event or response code of the container.
| uint32_t PIMA_Container_t::DataLength |
Length of the container and data, in bytes.
| uint32_t PIMA_Container_t::Params[3] |
Block parameters to be issued along with the block code (command blocks only).
| uint32_t PIMA_Container_t::TransactionID |
Unique container ID to link blocks together.
| uint16_t PIMA_Container_t::Type |
Container type, a value from the PIMA_Container_Types_t enum.