RNDIS Initialize Complete Message Structure.
More...
#include <RNDISClassCommon.h>
Type define for a RNDIS Initialize Complete response message.
- Note
- Regardless of CPU architecture, these values should be stored as little endian.
| uint32_t RNDIS_Initialize_Complete_t::AFListOffset |
| uint32_t RNDIS_Initialize_Complete_t::AFListSize |
| uint32_t RNDIS_Initialize_Complete_t::DeviceFlags |
| uint32_t RNDIS_Initialize_Complete_t::MajorVersion |
| uint32_t RNDIS_Initialize_Complete_t::MaxPacketsPerTransfer |
| uint32_t RNDIS_Initialize_Complete_t::MaxTransferSize |
| uint32_t RNDIS_Initialize_Complete_t::Medium |
| uint32_t RNDIS_Initialize_Complete_t::MessageLength |
| uint32_t RNDIS_Initialize_Complete_t::MessageType |
| uint32_t RNDIS_Initialize_Complete_t::MinorVersion |
| uint32_t RNDIS_Initialize_Complete_t::PacketAlignmentFactor |
| uint32_t RNDIS_Initialize_Complete_t::RequestId |
| uint32_t RNDIS_Initialize_Complete_t::Status |
The documentation for this struct was generated from the following file: