RNDIS Initialization Message Structure.
More...
#include <RNDISClassCommon.h>
Type define for a RNDIS Initialize command message.
- Note
- Regardless of CPU architecture, these values should be stored as little endian.
| uint32_t RNDIS_Initialize_Message_t::MajorVersion |
| uint32_t RNDIS_Initialize_Message_t::MaxTransferSize |
| uint32_t RNDIS_Initialize_Message_t::MessageLength |
| uint32_t RNDIS_Initialize_Message_t::MessageType |
| uint32_t RNDIS_Initialize_Message_t::MinorVersion |
| uint32_t RNDIS_Initialize_Message_t::RequestId |
The documentation for this struct was generated from the following file: