RNDIS Message Structure. More...
#include <RNDISClassCommon.h>
Data Fields | |
| uint32_t | DataLength |
| uint32_t | DataOffset |
| uint32_t | MessageLength |
| uint32_t | MessageType |
| uint32_t | NumOOBDataElements |
| uint32_t | OOBDataLength |
| uint32_t | OOBDataOffset |
| uint32_t | PerPacketInfoLength |
| uint32_t | PerPacketInfoOffset |
| uint32_t | Reserved |
| uint32_t | VcHandle |
Type define for a RNDIS packet message, used to encapsulate Ethernet packets sent to and from the adapter.
| uint32_t RNDIS_Packet_Message_t::DataLength |
| uint32_t RNDIS_Packet_Message_t::DataOffset |
| uint32_t RNDIS_Packet_Message_t::MessageLength |
| uint32_t RNDIS_Packet_Message_t::MessageType |
| uint32_t RNDIS_Packet_Message_t::NumOOBDataElements |
| uint32_t RNDIS_Packet_Message_t::OOBDataLength |
| uint32_t RNDIS_Packet_Message_t::OOBDataOffset |
| uint32_t RNDIS_Packet_Message_t::PerPacketInfoLength |
| uint32_t RNDIS_Packet_Message_t::PerPacketInfoOffset |
| uint32_t RNDIS_Packet_Message_t::Reserved |
| uint32_t RNDIS_Packet_Message_t::VcHandle |