RNDIS OID Property Query Message Structure.
More...
#include <RNDISClassCommon.h>
Type define for a RNDIS OID Property Query command message.
- Note
- Regardless of CPU architecture, these values should be stored as little endian.
| uint32_t RNDIS_Query_Message_t::DeviceVcHandle |
| uint32_t RNDIS_Query_Message_t::InformationBufferLength |
| uint32_t RNDIS_Query_Message_t::InformationBufferOffset |
| uint32_t RNDIS_Query_Message_t::MessageLength |
| uint32_t RNDIS_Query_Message_t::MessageType |
| uint32_t RNDIS_Query_Message_t::Oid |
| uint32_t RNDIS_Query_Message_t::RequestId |
The documentation for this struct was generated from the following file: