SCSI Device LUN Capacity Structure. More...
#include <MassStorageClassHost.h>
Data Fields | |
| uint32_t | Blocks |
| uint32_t | BlockSize |
SCSI capacity structure, to hold the total capacity of the device in both the number of blocks in the current LUN, and the size of each block. This structure is filled by the device when the MS_Host_ReadDeviceCapacity() function is called.
| uint32_t SCSI_Capacity_t::Blocks |
Number of blocks in the addressed LUN of the device.
| uint32_t SCSI_Capacity_t::BlockSize |
Number of bytes in each block in the addressed LUN.